Part Number: PROCESSOR-SDK-TDAX
Hi
I am using the SFM algorithm for fcw.
we don't have an external sensor mounted to car, e.g. IMU.
So we do not want to use Camera Extrinsic Parameters.
I reviewed the camExtPrm variable in StructureFromMotion_DSP_UserGuide.pdf to disable the Camera Extrinsic Parameters .
Field : camExtPrm, Data Type : Float[]
Description :
Camera Extrinsic Parameters. Format of camera extrinsic parameters is [ r00 r01 r02 t0 r10 r11 r12 t1 r20 r21 r22 t2], where rij are the rotation parameter, and ti are the translation parameter. If this pointer is provided as NULL, then these parameters are computed internally
camExtPrm variable is floa camExtPrm[SFM_TI_CAMERA_EXTRENSIC_PARAM_SIZE];
How do i set a camExtPrm variable to compute internally?
Regards
JP Park