This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Application loading at bootup

Part Number: RTOS

Tool/software: TI-RTOS

Hi

I am using evmAM5728 board and I use CCS v8 (windows) and built VIP loopback example and generated .out using RTOS SDK(processor_sdk_rtos_am57xx_5_00_00_15). Now I want to load .out into the board ,so I can run the program after the power is on again. 

When I searched for that I found it can done using boot process using SBL

Step 1. to create Bootable SDCard

2.Copy app and MLO files into SDCard

3.Insert the SDCard into EVM and power on.

Can I copy the app file generated under vip ccs project Debug path into SD Card at the boot up, will it work?

Please correct me if I am wrong.

Thanks,

Jahnavi