Other Parts Discussed in Thread: OMAP-L138
Hi,
I would like to check if L138 ARM bootloader make any assumption on the pin connection ?
From "Using the OMAP-L1x8 Bootloader (SPRAB41C)", if understand correctly, there is such requirement on the connection.
See section 6 Master Boot – Booting From a Slave Memory Device:
…
For booting from a NOR Flash, a configuration word is required before AIS as shown in Figure 3. NOR Flash should be connected to EMA_CS[2] of the EMIFA peripheral.
…
NAND Flash should be connected to EMA_CS[3] of the EMIFA peripheral. The ALE and CLE pins of the NAND device should be connected to the EMA_A[1] and EMA_A[2] pins of the EMIFA peripheral,respectively. Complete details of supported NAND devices are available in Appendix B.
rgds,
kc Wong