This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H14: Long Trace Lengths on High-speed Signals

Part Number: 66AK2H14
Other Parts Discussed in Thread: DS64BR111, DS64BR401, DS80PCI402, DS80PCI102

Hello, the max trace lengths for PCIe is 15-inches and SGMII is about 20-inches. If you are unable to get below that limit is there some kind of driver one could use on the TX pairs? I have about 9-inches from processor to a backplane connector and then about 2-inches of backplane traces back up to another card, so I'm getting pretty close to the limit. Can anyone suggest a solution?

Last, the trace limit for SRIO is 30-inches with 8mil traces, but I'm using 4-min traces so would would be the limit in that case for SRIO traces?

Thanks,

Joe