Part Number: AM4378
Tool/software: Linux
I have a simple LKM that as of right now just has init and exit functions that each only have a single printk statement inside them. I am able to build this LKM against the kernel using a Makefile, but when I try to insmod it on the AM437x EVM board, a ton of errors are output:
[ 85.560199] Unable to handle kernel paging request at virtual address 7e6f426c
[ 85.567700] pgd = edb20000
[ 85.570439] [7e6f426c] *pgd=00000000
[ 85.579318] Internal error: Oops: 5 [#1] PREEMPT ARM
[ 85.584322] Modules linked in: UTI_ring_detect_driver(O+) sha512_generic sha512_arm sha256_generi)
[ 85.652180] CPU: 0 PID: 979 Comm: insmod Tainted: G O 4.9.69-g9ce43c71ae #1
[ 85.660319] Hardware name: Generic AM43 (Flattened Device Tree)
[ 85.666282] task: edb50b00 task.stack: edbac000
[ 85.670863] PC is at load_module+0x1c0c/0x2180
[ 85.675343] LR is at load_module+0x1bf8/0x2180
[ 85.679825] pc : [<c01978c4>] lr : [<c01978b0>] psr: 30070013
[ 85.679825] sp : edbade60 ip : edbade60 fp : edbadf1c
[ 85.691371] r10: 00000007 r9 : 00000000 r8 : edb42ca8
[ 85.696630] r7 : 7e6f4258 r6 : bf37a0c0 r5 : bf37a0cc r4 : edbadf44
[ 85.703196] r3 : bf37a260 r2 : 00000000 r1 : 00000000 r0 : c0c16440
[ 85.709768] Flags: nzCV IRQs on FIQs on Mode SVC_32 ISA ARM Segment none
[ 85.716949] Control: 10c53c7d Table: adb20059 DAC: 00000051
[ 85.722733] Process insmod (pid: 979, stack limit = 0xedbac208)
[ 85.728689] Stack: (0xedbade60 to 0xedbae000)
[ 85.733091] de60: bf37a0cc 00007fff bf37a0c0 c0194e74 bf000000 c099ce6c c099ce44 c099ce9c
[ 85.741330] de80: c099ce38 c08045bc bf37a0cc f23477b4 bf37a260 edbadf44 bf37a108 bf37a1d4
[ 85.749567] dea0: edbadeec edbadeb0 c021d190 c021cadc f2347000 00000000 00000000 00000000
[ 85.757801] dec0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 85.766036] dee0: 00000000 00000000 00000000 00000000 7fffffff 00000000 00000003 00027dc4
[ 85.774272] df00: 0000017b c0107e84 edbac000 00000000 edbadfa4 edbadf20 c0198058 c0195cc4
[ 85.782507] df20: 7fffffff 00000000 00000003 edbadf38 c01dc790 f2347000 00000b80 00000000
[ 85.790742] df40: 00000000 f2347000 00000b80 f23474e4 f2347421 f2347a74 00000280 00000310
[ 85.798977] df60: 00000000 00000000 00000000 0000035c 00000012 00000013 0000000a 00000008
[ 85.807211] df80: 00000006 00000000 00000000 0003a008 00000000 00025a74 00000000 edbadfa8
[ 85.815446] dfa0: c0107cc0 c0197fb4 0003a008 00000000 00000003 00027dc4 00000000 00000000
[ 85.823680] dfc0: 0003a008 00000000 00025a74 0000017b 00000000 00000002 b6f21000 00000000
[ 85.831917] dfe0: beb1fb08 beb1faf8 0001f57c b6e6b9f2 80070030 00000003 80030064 6d800906
[ 85.840134] Backtrace:
[ 85.842632] [<c0195cb8>] (load_module) from [<c0198058>] (SyS_finit_module+0xb0/0xc0)
[ 85.850525] r10:00000000 r9:edbac000 r8:c0107e84 r7:0000017b r6:00027dc4 r5:00000003
[ 85.858398] r4:00000000
[ 85.860982] [<c0197fa8>] (SyS_finit_module) from [<c0107cc0>] (ret_fast_syscall+0x0/0x48)
[ 85.869212] r6:00025a74 r5:00000000 r4:0003a008
[ 85.873874] Code: e51b308c e1530007 e2477008 0a000009 (e5973014)
[ 85.897747] ---[ end trace b2596d9f564123af ]---
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.579318] Internal error: Oops: 5 [#1] PREEMPT ARM
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.722733] Process insmod (pid: 979, stack limit = 0xedbac208)
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.728689] Stack: (0xedbade60 to 0xedbae000)
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.733091] de60: bf37a0cc 00007fff bf37a0c0 c0194e74 bf000000 c099ce6c c099ce44 c09c
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.741330] de80: c099ce38 c08045bc bf37a0cc f23477b4 bf37a260 edbadf44 bf37a108 bf34
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.749567] dea0: edbadeec edbadeb0 c021d190 c021cadc f2347000 00000000 00000000 0000
Segmentation fault
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.757801] dec0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 0000
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.766036] dee0: 00000000 00000000 00000000 00000000 7fffffff 00000000 00000003 0004
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.774272] df00: 0000017b c0107e84 edbac000 00000000 edbadfa4 edbadf20 c0198058 c014
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.782507] df20: 7fffffff 00000000 00000003 edbadf38 c01dc790 f2347000 00000b80 0000
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.790742] df40: 00000000 f2347000 00000b80 f23474e4 f2347421 f2347a74 00000280 0000
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.798977] df60: 00000000 00000000 00000000 0000035c 00000012 00000013 0000000a 0008
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.807211] df80: 00000006 00000000 00000000 0003a008 00000000 00025a74 00000000 edb8
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.815446] dfa0: c0107cc0 c0197fb4 0003a008 00000000 00000003 00027dc4 00000000 0000
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.823680] dfc0: 0003a008 00000000 00025a74 0000017b 00000000 00000002 b6f21000 0000
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.831917] dfe0: beb1fb08 beb1faf8 0001f57c b6e6b9f2 80070030 00000003 80030064 6d86
Broadcast message from systemd-journald@am437x-evm (Wed 2018-10-24 19:39:20 UTC):
kernel[378]: [ 85.873874] Code: e51b308c e1530007 e2477008 0a000009 (e5973014)
Any idea why is this happening?