This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AM5728: Bootstrap the C66xx DSP on the AM5728 with no TI-RTOS (only bare-metal code)

Part Number: AM5728

Tool/software: TI-RTOS

Hi,

I intend to write bare metal code for one of the DSPs on the AM5728. I am running Linux on the A15 core and need to bootstrap the DSP using the rproc interface. Can this be done? If so, please can you point me to some documentation or some examples?

Thanks very much.

Regards,

Shaunak

  • Hi, Shaunak,

    Unfortunately, this use case is not supported, and we don't have either examples nor documentation on it.
    If you consider running RTOS application on DSP, we have several examples and also documentation for it.

    Rex