Other Parts Discussed in Thread: TPS3110
Is a rising edge necessary for nRESET? Due to an error in the PCB the nRESET Pin is floating, to correct this without redesign it is now connected to 3,3V with a wire under the BGA. The nPOR Pin is connected to an TPS3110 and is working properly. The DM648 should boot from flash, but there is no AECLKOUT and no nACE2 signal. Configuration pins are ok.
AEA11 1k PDN
AEA12 1k PDN
AEA13 1k PUP
AEA14 1k PDN
AEA15 1k PUP
AEA17 1k PUP
AEA20 1k PUP
AEA21 1k PDN
AEA22 1k PUP
UHPIEN 3,3V
I am not able to connect to SYSCLK4 for measurement, CLKIN1, CLKIN2 and BECLKOUT are ok.
PS: Sorry for my english.