The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6747: AISgen tool and CCS 7.4 for C6747

Part Number: TMS320C6747

Tool/software: Code Composer Studio

Hi,


I have one question regarding DSP C6747 and tool.

My customer had developed C6747 unique board based on the below environment.

HOST OS : Windows XP
CCS ver.:  3.3
AISgen D800K001

This time, customer will have a plan to update their development environment as the below.
HOST OS : Window10(64bit)
CCS ver.: 7.4
AISgen D800K008

My question is the below.


1) AISgen D800K008. Is this latest version for AIS generation? Or is there later version?

2) Can the .out file that is made by CCS7.4(Customer will migrate their program from CCS3.3 to CCS7.4) be used for the latest AISgen (D800K008?)?

3) From D800K001 to D800K008, GUI seems to be changed any point. Is the all features of D800K001 included in D800K008?
The attached file is the customer configuration for D800K001. Are these settings available on D800K008?

4) Is there any information of migration from CCS3.3 to CCS7.4? What are the points to be noted for C6747?

I appreciate your quick reply.

Best regards,

Michi