Part Number: OMAP-L138
Hi,
I've been using the OMAP-L138 power consumption spreadsheet provided here 'processors.wiki.ti.com/.../OMAP-L138_Power_Consumption_Summary have a question about the power consumption of the Timer modules.
Timers 0 and 1 are driven from PLL0_AUXCLK which is OSCIN lets say 24MHz.
Timers 2 and 3 are driven from PLL0_SYSCLK2 or PLL1_SYSCLK2 which will typically have a much higher frequency.
The spreadsheet says for the Timer 0/1 frequency fields 'Program this field with the timer frequency in MHz (max value of 12MHz).'. What is this frequency? Is it the module frequency (in that case limiting to 12MHz seems odd) or the timer period as a frequency or something else?
If the spreadsheet is configured for 'Typical - 456MHz' using the button at the bottom and then I set Timer 0 to have a frequency of 1MHz the spreadsheet says the timer takes 8.2mW that seems a lot considering there is no I/O and it is just counting up. It's more than a SPI device running at 27MHz, 100% utilisation. Is there a bug in the spreadsheet or does the timer really take this much power? Also entering anything below 12MHz results in the same power consumption of 8.2mW, when you enter 12MHz it jumps to 12.4mW.
Thanks
Nigel