Other Parts Discussed in Thread: TPS65920, OMAP3530
Hi,
I am using the TPS65920 with an OMAP3530.
I want to use the USB either as a host, or as a device, but not the OTG features. The mode will be decided by the OMAP.
In device mode, I have system requirements that prevent me from connecting the VBUS from the external host to VBUS of the PMIC.
If the system knows in advance it has to run as a device, does the protocol/ the hardware require a +5V on VBUS, or can it handle a proper communication only with D+/D-/ GND ?
Would the absence of VBUS need driver modifications ?
Regards
Philippe