This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3: Memory Mapping Issue.

Part Number: TDA3

Hi Sir,

As per the memory mapping  OCMC RAM area (0x4030_0000) is mapped to the 0x0030_0000 virtual address space. So my thinking is that data at address 0x4030_0000 should be same as data at address 0x0030_0000. Is it correct? If it is right then why these content are different?

Physical memory data is changed after read data from SDF via EDMA. At some location it is reflecting correctly. 

What should I do to reflect the same data at both location?

Thanks in Advance!

Thank You,
Sagar K