Hi folks,
I have a custom board based on the VC5509A DSP. The board has a 3.5' QVGA TFT LCD( with integrated controller) attached to EMIF of the DSP. I also have a 2GB SD card on MMC/SD controller.
Now I wanted to implement a video decoder in software and run on the DSP. My question is can the DSP handle basic video decoding running at 200MHz?
in addition; I have an ARM7TDMI MPU on board, connected through SPI with the DSP, in case it helps
PS: I'm new to video decoding and stuff, but I've a lot of experience with 5509A