This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6446 reset problem!

I used u-boot-1.1.4, but when I ran its 'reset' command, the board hanged, why?

I don't modify any u-boot-1.1.4 source codes .

  • Are you referring to the u-boot or Linux 'reset command'?  I assume u-boot. 

    I was able to find a 'reset' u-boot bug associated with our older u-boot (I could not readily find the version), but this should be fixed in our newer u-boot release.  FYI, latest DVSDK includes u-boot 1.20

  • Hi, Juan

    I've also encounted this problem. and the worse is there are no messages displayed in the HyperTermial when the DM6446 EVM is powered on.

    Actually I used 2 commands "erase all" and "reset" in the U-boot shell, and after that the U-boot didn't boot.

    BR.

    Yulin 

    P.S. the previous boot information is attached here.

    DaVinci EVM # printenv
    bootcmd=setenv setboot setenv bootargs $(bootargs) video=dm64xxfb:output=$(video
    std);run setboot;bootm 0x2050000
    bootdelay=3
    baudrate=115200
    bootfile="uImage"
    _ipaddr  nv=ipaddr=NULL
    ipaddr=192.168.0.188
    serverip=192.168.0.49
    netmask=255.255.255.0
    gatewayip=192.168.0.1
    nfshost=192.168.0.49
    rootpath=/home/160syl/dm6446/nfs_rootfs
    bootargs=console=ttyS0,115200n8 noinitrd rw ip=192.168.0.188:192.168.0.49:192.16
    8.0.1:255.255.255.0:eth0 root=/dev/nfs nfsroot=192.168.0.49:/home/160syl/dm6446/
    nfs_rootfs,nolock mem=120M
    stdin=serial
    stdout=serial
    stderr=serial
    ethaddr=00:0e:99:02:55:8b
    videostd=ntsc

    Environment size: 663/65532 bytes
    DaVinci EVM # saveenv
    Saving Environment to Flash...
    Un-Protected 1 sectors
    Erasing Flash...
    Erasing sector  4 ... done.
     Erase Operation Completed.
    Erased 1 sectors
    Writing to Flash...-done
    Protected 1 sectors
    DaVinci EVM # reset


    U-Boot 1.1.3 (Mar 15 2006 - 11:42:19)

    U-Boot code: 81080000 -> 81097320  BSS: -> 810A0230
    RAM Configuration:
    Bank #0: 80000000 256 MB
    MY AMD Flash: 16 MB
    In:    serial
    Out:   serial
    Err:   serial
    ARM Clock :- 283MZ
    DDR Clock :- 189MZ
    Hit any key to stop autoboot:  0
    DaVinci EVM # reset


    U-Boot 1.1.3 (Mar 15 2006 - 11:42:19)

    U-Boot code: 81080000 -> 81097320  BSS: -> 810A0230
    RAM Configuration:
    Bank #0: 80000000 256 MB
    MY AMD Flash: 16 MB
    In:    serial
    Out:   serial
    Err:   serial
    ARM Clock :- 283MZ
    DDR Clock :- 189MZ
    Hit any key to stop autoboot:  0
    DaVinci EVM # erase start end
    Bad address format
    DaVinci EVM # erase all
    Erase Flash Bank # 1 - Warning: 1 protected sectors will not be erased!
    Erasing sector  0 ... done.
    Erasing sector  1 ... done.
    Erasing sector  2 ... done.
    Erasing sector  3 ... done.
    Erasing sector  5 ... done.
    Erasing sector  6 ... done.
    Erasing sector  7 ... done.
    Erasing sector  8 ... done.
    Erasing sector  9 ... done.
    Erasing sector 10 ... done.
    Erasing sector 11 ... done.
    Erasing sector 12 ... done.
    Erasing sector 13 ... done.
    Erasing sector 14 ... done.
    Erasing sector 15 ... done.
    Erasing sector 16 ... done.
    Erasing sector 17 ... done.
    Erasing sector 18 ... done.
    Erasing sector 19 ... done.
    Erasing sector 20 ... done.
    Erasing sector 21 ... done.
    Erasing sector 22 ... done.
    Erasing sector 23 ... done.
    Erasing sector 24 ... done.
    Erasing sector 25 ... done.
    Erasing sector 26 ... done.
    Erasing sector 27 ... done.
    Erasing sector 28 ... done.
    Erasing sector 29 ... done.
    Erasing sector 30 ... done.
    Erasing sector 31 ... done.
    Erasing sector 32 ... done.
    Erasing sector 33 ... done.
    Erasing sector 34 ... done.
    Erasing sector 35 ... done.
    Erasing sector 36 ... done.
    Erasing sector 37 ... done.
    Erasing sector 38 ... done.
    Erasing sector 39 ... done.
    Erasing sector 40 ... done.
    Erasing sector 41 ... done.
    Erasing sector 42 ... done.
    Erasing sector 43 ... done.
    Erasing sector 44 ... done.
    Erasing sector 45 ... done.
    Erasing sector 46 ... done.
    Erasing sector 47 ... done.
    Erasing sector 48 ... done.
    Erasing sector 49 ... done.
    Erasing sector 50 ... done.
    Erasing sector 51 ... done.
    Erasing sector 52 ... done.
    Erasing sector 53 ... done.
    Erasing sector 54 ... done.
    Erasing sector 55 ... done.
    Erasing sector 56 ... done.
    Erasing sector 57 ... done.
    Erasing sector 58 ... done.
    Erasing sector 59 ... done.
    Erasing sector 60 ... done.
    Erasing sector 61 ... done.
    Erasing sector 62 ... done.
    Erasing sector 63 ... done.
    Erasing sector 64 ... done.
    Erasing sector 65 ... done.
    Erasing sector 66 ... done.
    Erasing sector 67 ... done.
    Erasing sector 68 ... done.
    Erasing sector 69 ... done.
    Erasing sector 70 ... done.
    Erasing sector 71 ... done.
    Erasing sector 72 ... done.
    Erasing sector 73 ... done.
    Erasing sector 74 ... done.
    Erasing sector 75 ... done.
    Erasing sector 76 ... done.
    Erasing sector 77 ... done.
    Erasing sector 78 ... done.
    Erasing sector 79 ... done.
    Erasing sector 80 ... done.
    Erasing sector 81 ... done.
    Erasing sector 82 ... done.
    Erasing sector 83 ... done.
    Erasing sector 84 ... done.
    Erasing sector 85 ... done.
    Erasing sector 86 ... done.
    Erasing sector 87 ... done.
    Erasing sector 88 ... done.
    Erasing sector 89 ... done.
    Erasing sector 90 ... done.
    Erasing sector 91 ... done.
    Erasing sector 92 ... done.
    Erasing sector 93 ... done.
    Erasing sector 94 ... done.
    Erasing sector 95 ... done.
    Erasing sector 96 ... done.
    Erasing sector 97 ... done.
    Erasing sector 98 ... done.
    Erasing sector 99 ... done.
    Erasing sector 100 ... done.
    Erasing sector 101 ... done.
    Erasing sector 102 ... done.
    Erasing sector 103 ... done.
    Erasing sector 104 ... done.
    Erasing sector 105 ... done.
    Erasing sector 106 ... done.
    Erasing sector 107 ... done.
    Erasing sector 108 ... done.
    Erasing sector 109 ... done.
    Erasing sector 110 ... done.
    Erasing sector 111 ... done.
    Erasing sector 112 ... done.
    Erasing sector 113 ... done.
    Erasing sector 114 ... done.
    Erasing sector 115 ... done.
    Erasing sector 116 ... done.
    Erasing sector 117 ... done.
    Erasing sector 118 ... done.
    Erasing sector 119 ... done.
    Erasing sector 120 ... done.
    Erasing sector 121 ... done.
    Erasing sector 122 ... done.
    Erasing sector 123 ... done.
    Erasing sector 124 ... done.
    Erasing sector 125 ... done.
    Erasing sector 126 ... done.
    Erasing sector 127 ... done.
    Erasing sector 128 ... done.
    Erasing sector 129 ... done.
    Erasing sector 130 ... done.
    Erasing sector 131 ... done.
    Erasing sector 132 ... done.
    Erasing sector 133 ... done.
    Erasing sector 134 ... done.
    Erasing sector 135 ... done.
    Erasing sector 136 ... done.
    Erasing sector 137 ... done.
    Erasing sector 138 ... done.
    Erasing sector 139 ... done.
    Erasing sector 140 ... done.
    Erasing sector 141 ... done.
    Erasing sector 142 ... done.
    Erasing sector 143 ... done.
    Erasing sector 144 ... done.
    Erasing sector 145 ... done.
    Erasing sector 146 ... done.
    Erasing sector 147 ... done.
    Erasing sector 148 ... done.
    Erasing sector 149 ... done.
    Erasing sector 150 ... done.
    Erasing sector 151 ... done.
    Erasing sector 152 ... done.
    Erasing sector 153 ... done.
    Erasing sector 154 ... done.
    Erasing sector 155 ... done.
    Erasing sector 156 ... done.
    Erasing sector 157 ... done.
    Erasing sector 158 ... done.
    Erasing sector 159 ... done.
    Erasing sector 160 ... done.
    Erasing sector 161 ... done.
    Erasing sector 162 ... done.
    Erasing sector 163 ... done.
    Erasing sector 164 ... done.
    Erasing sector 165 ... done.
    Erasing sector 166 ... done.
    Erasing sector 167 ... done.
    Erasing sector 168 ... done.
    Erasing sector 169 ... done.
    Erasing sector 170 ... done.
    Erasing sector 171 ... done.
    Erasing sector 172 ... done.
    Erasing sector 173 ... done.
    Erasing sector 174 ... done.
    Erasing sector 175 ... done.
    Erasing sector 176 ... done.
    Erasing sector 177 ... done.
    Erasing sector 178 ... done.
    Erasing sector 179 ... done.
    Erasing sector 180 ... done.
    Erasing sector 181 ... done.
    Erasing sector 182 ... done.
    Erasing sector 183 ... done.
    Erasing sector 184 ... done.
    Erasing sector 185 ... done.
    Erasing sector 186 ... done.
    Erasing sector 187 ... done.
    Erasing sector 188 ... done.
    Erasing sector 189 ... done.
    Erasing sector 190 ... done.
    Erasing sector 191 ... done.
    Erasing sector 192 ... done.
    Erasing sector 193 ... done.
    Erasing sector 194 ... done.
    Erasing sector 195 ... done.
    Erasing sector 196 ... done.
    Erasing sector 197 ... done.
    Erasing sector 198 ... done.
    Erasing sector 199 ... done.
    Erasing sector 200 ... done.
    Erasing sector 201 ... done.
    Erasing sector 202 ... done.
    Erasing sector 203 ... done.
    Erasing sector 204 ... done.
    Erasing sector 205 ... done.
    Erasing sector 206 ... done.
    Erasing sector 207 ... done.
    Erasing sector 208 ... done.
    Erasing sector 209 ... done.
    Erasing sector 210 ... done.
    Erasing sector 211 ... done.
    Erasing sector 212 ... done.
    Erasing sector 213 ... done.
    Erasing sector 214 ... done.
    Erasing sector 215 ... done.
    Erasing sector 216 ... done.
    Erasing sector 217 ... done.
    Erasing sector 218 ... done.
    Erasing sector 219 ... done.
    Erasing sector 220 ... done.
    Erasing sector 221 ... done.
    Erasing sector 222 ... done.
    Erasing sector 223 ... done.
    Erasing sector 224 ... done.
    Erasing sector 225 ... done.
    Erasing sector 226 ... done.
    Erasing sector 227 ... done.
    Erasing sector 228 ... done.
    Erasing sector 229 ... done.
    Erasing sector 230 ... done.
    Erasing sector 231 ... done.
    Erasing sector 232 ... done.
    Erasing sector 233 ... done.
    Erasing sector 234 ... done.
    Erasing sector 235 ... done.
    Erasing sector 236 ... done.
    Erasing sector 237 ... done.
    Erasing sector 238 ... done.
    Erasing sector 239 ... done.
    Erasing sector 240 ... done.
    Erasing sector 241 ... done.
    Erasing sector 242 ... done.
    Erasing sector 243 ... done.
    Erasing sector 244 ... done.
    Erasing sector 245 ... done.
    Erasing sector 246 ... done.
    Erasing sector 247 ... done.
    Erasing sector 248 ... done.
    Erasing sector 249 ... done.
    Erasing sector 250 ... done.
    Erasing sector 251 ... done.
    Erasing sector 252 ... done.
    Erasing sector 253 ... done.
    Erasing sector 254 ... done.
    Erasing sector 255 ... done.
     Erase Operation Completed.
    DaVinci EVM # print
    bootcmd=setenv setboot setenv bootargs $(bootargs) video=dm64xxfb:output=$(video
    std);run setboot;bootm 0x2050000
    bootdelay=3
    baudrate=115200
    bootfile="uImage"
    _ipaddr  nv=ipaddr=NULL
    ipaddr=192.168.0.188
    serverip=192.168.0.49
    netmask=255.255.255.0
    gatewayip=192.168.0.1
    nfshost=192.168.0.49
    rootpath=/home/160syl/dm6446/nfs_rootfs
    bootargs=console=ttyS0,115200n8 noinitrd rw ip=192.168.0.188:192.168.0.49:192.16
    8.0.1:255.255.255.0:eth0 root=/dev/nfs nfsroot=192.168.0.49:/home/160syl/dm6446/
    nfs_rootfs,nolock mem=120M
    stdin=serial
    stdout=serial
    stderr=serial
    ethaddr=00:0e:99:02:55:8b
    videostd=ntsc

    Environment size: 663/65532 bytes
    DaVinci EVM # reset 

     

  • Hi,

    Have you tried newer u-boot? I think the problem has been fixed.

  • Hi, Paul

    Thank you for your reply.

    This problem has been fixed by following these steps.

    1. Flash the newer u-boot file "u-boot-567-nor_s3_4_fix.bin" by using "DVFlasher_1_10.exe" through UART.

    2. Burn the "uImage" to NOR flash by using the following commands and the S3 should be "1111111111" when burning. 

        DaVinci EVM # tftpboot 0x80080000 uImage

        DaVinci EVM # erase 0x2050000 22fffff 

        DaVinci EVM # cp.b 0x80080000 0x2050000 0x200000

    However, I can't find the verify answer button below probably because I'm not the starter of this post, so sorry for that.

    BR.

    Yulin 

    P.S. I tried the u-boot-1.2.0, but there are no responses in Hyperterminal, does this version of u-boot not  match TMDXEVM6446?