Tool/software: Linux
Hi TI,
I run PSDKLA3.4 in tda2x evm. Because I want to run the QT app in it.
But the weston can't start up.like this:
root@dra7xx-evm:~# root@dra7xx-evm:~# cat /var/log/weston.log Date: 2018-10-23 UTC [07:36:18.772] weston 1.9.0 http://wayland.freedesktop.org Bug reports to: bugs.freedesktop.org/enter_bug.cgi Build: 1.8.93-2-gb05cdb8 configure.ac: bump to version 1.9.0 for the official release (2015-09-21 18:11:26 -0700) [07:36:18.772] OS: Linux, 4.4.84-00027-g018eb62-dirty, #7 SMP PREEMPT Sat Sep 29 11:18:05 HKT 2018, armv7l [07:36:18.775] Using config file '/etc//weston.ini' [07:36:18.779] Loading module '/usr/lib/weston/drm-backend.so' [07:36:18.862] Output repaint window is 7 ms maximum. [07:36:18.862] initializing drm backend [07:36:18.865] using /dev/dri/card0 [07:36:18.867] Loading module '/usr/lib/weston/gl-renderer.so' loaded module : gbm_pvr.so found valid GBM backend : gbm_pvr.so [07:36:19.175] warning: either no EGL_EXT_platform_base support or specific platform support; falling back to eglGetDisplay. [07:36:19.205] failed to initialize display [07:36:19.205] EGL error state: EGL_BAD_ALLOC (0x3003) [07:36:19.205] failed to initialize egl [07:36:19.205] fatal: failed to create compositor backend PVR:(Error): OpenServices: PVRDRMOpenRender failed [0, ] PVR:(Error): PVRSRVConnect: Unable to open connection. [0, ] PVR:(Error): Couldn't connect to services [0, ] root@dra7xx-evm:~# root@dra7xx-evm:~#
and the /etc/powervr.ini is :
root@dra7xx-evm:~# root@dra7xx-evm:~# cat /etc/powervr.ini [default] #WindowSystem=libpvrws_WAYLAND.so [weston] DbmDriverName=vdrm [weston-simple-egl] DbmDriverName=vdrm #QT app [animatedtiles] DbmDriverName=vdrm root@dra7xx-evm:~# root@dra7xx-evm:~#
And I have add the cma=128M.
Have any suggestions ? Thanks!
Regards,
Sam.