This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel and CF Card

Hallo!

I have a costimized DM6446 which works with MVL 4. The RFS is placed on a CF-Card.

Boot Messages:

...

Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2

ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx

MUX: initialized HDIREN

MUX: initialized ATAEN

hda: CF Card, ATA DISK drive

elevator: using anticipatory as default io scheduler

ide0 at 0xe10661f0-0xe10661f7,0xe10663f6 on irq 22

hda: max request size: 128KiB

hda: 3940272 sectors (2017 MB) w/1KiB Cache, CHS=3909/16/63

hda: hda1

 

..

 

Now I want to use MVL 5. I compiled the kernel (described in SPRUE66F 4.5) with CF-Card support enabled. But when the kernel boots, it doesn't

find any CF-Card. Only tries to mount a file system in flash. I tried with the pre-compiled  kernel "uImage-ti-davinci_evm-arm_v5t_le", same result.

Does anybody know what the problem is? Why the new kernel doesn't find the CF-Card?

Thanks