This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4376: GPIOs with mixed power supply

Part Number: AM4376

Hello

I'm using the AM4376 processor in our design. My GPIO bank power supplies are mixed between 3.3VDC and 1.8VDC. Is it acceptable to have mixed I/O supplies for the GPIO banks and ignore the warnings as long as the GPIOs are used with logic levels that correspond to the supply voltage? The example below is from our design where the GPIO bank 0 is powered by BDDSHV9 (3.3V) BDDSHV3 (1.8V) and BDDSHV6 (3.3V). so I'm using GPIOs powered by the BDDSHV9 and BDDSHV6 at the 3.3VDC logic levels and the GPIOs powered by the BDDSHV3 at the 1.8VDC logic levels.

# Design Signal
Pad Name
PUPD State
 During HHV
PUPD State
 After HHV
IO Power
Supply
Name
IO
Power
Setting
Required
Voltage
Level
Ball
Name
Selected Mode Number Mode
Interface
 Name
Mode
Signal
 Name
User
Requirement
 Name
1 gpmc_clk PD PD VDDSHV9 3.3V 1.8V A12 9 GPIO0 gpio0[4] MyGPIO0
2 spi0_cs1 OFF PU VDDSHV3 1.8V 1.8V R25 7 GPIO0 gpio0[6] MyGPIO0
3 eCAP0_in_PWM0_out OFF PD VDDSHV3 1.8V 1.8V G24 7 GPIO0 gpio0[7] MyGPIO0
4 dss_data12 OFF OFF VDDSHV6 3.3V 1.8V C19 7 GPIO0 gpio0[8] MyGPIO0
5 dss_data13 OFF OFF VDDSHV6 3.3V 1.8V D19 7 GPIO0 gpio0[9] MyGPIO0
6 dss_data14 OFF OFF VDDSHV6 3.3V 1.8V C17 7 GPIO0 gpio0[10] MyGPIO0

regards

Khalid