This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H12: About doorbell interrupt setting for SRIO

Part Number: 66AK2H12

Hi,

I'd like to use the doorbell interrupt to determine two different events separately.
For example, when the transmission side has set the event A and the event B as follows:

[SRIO transmission side]
Event A setting:
  info.DoorBellReg = 00b
  info.DoorBellbit = 0000b
 
Event B setting:
  info.DoorBellReg = 00b
  info.DoorBellbit = 0001b


By checking ICS0 or ICS1 on the receiving side, I think that it is possible to judge which event is occurring.

[SRIO receiving side]
if ICS0 of DoorBell[0] occurred --> So, the receiving side can judge that the event A has occurred.
if ICS1 of DoorBell[0] occurred --> So, the receiving side can judge that the event B has occurred.


Is my understanding correct?


Best Regards,
H.U