This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP2430SDP Linux and bootloaders

Where could I find information on Linux and bootloader source code that was the last supported 2430 software by TI?  I"m assuming I can grab the omap2430SDP linux build from Angstrom/Openembedded and also an older uboot, but I wanted to be sure that TI didn't have a revision controlled version that I could start with.  Also is a xloader required, or is the 2430 able to single stage boot?

Also, these are the only instructions I've found with how to load the SDP with Linux, are there others?

http://linux.omap.com/pipermail/linux-omap-open-source/2007-January/008841.html