This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: CPU load measurement

Part Number: AM5728


Tool/software: Linux

Hi,

Is it possible to measure the CPU load of IVAHD or IPU when executing encode or decode?
In the Processor SDK linux there are the following commands to check the load of each core, but there seems to be no such two things.
Since IVAHD is a coprocessor, it may not be, but please tell me.
ARM: top command
DSP: dsptop command
GPU: pvrscope command
IPU?
IVAHD?

Best Regards,
Shigehiro Tsuda