This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can Omap137 EMA_clk output as clock signal?



I want to output EMA_clk  interfcing to cpld as a clock signal.when i use ccs3.3 to make a test,I found EMA_clk is ok when CCS is setup.i can detect it with oscillograph But while dsp is runing I cann't detect  EMA_clk with oscillograph . I can read and write  flash in EMIFA CS3 correctly,then i think EMA_clk may be work,But how can't idetect it with oscillograph ?

Second question about  using  ccs3.3 . when I write to EMIFA CS4 ,actually EMIFA CS4 interface no memories,I can see the memories in CCS  VIEW->Memory,I was confused ,because this memory space is not exist at all