Part Number: AMIC110
Other Parts Discussed in Thread: AM3357
Hi Sitara support Team,
Can EtherCAT Slave controller on AM3357/AMIC110 detect the error of FCS?
My customer needs to measure the number of "malformed packets"
for checking the effect of the NOISE-COUNTERMEASURE.
They captured the packets with the Hilscher netAnalyzer as follows connection.
EtherCAT master sends a malformed FCS (Frame Check Sequence) packet(No.9).
However, EtherCAT slaves1 to slave4 receive the packet and seem to return to
the next packet(No.10) correctly updated the working counter.
Please refer to the pcap file.
detect_NG.zip
If TI's EtherCAT slave controller does not have the function to detect the error of FCS,
is there any alternative function?
Best regards,
Kanae