Hi
In AM335X can we have control over the GPIO from the Pre boot-loader level(from spl)
Regards
Eby
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM3356
Hi,
I am using AM3356 processor. We want to use a GPIO at the SPL level. Once it is being used during SPL Execution, it should not be accessed from the Uboot or kernel. Is it possible to implement such thing?
Also, whether a write protect (WP) can be overwritten from JTAG?
kushal banerjee said:I am using AM3356 processor. We want to use a GPIO at the SPL level. Once it is being used during SPL Execution, it should not be accessed from the Uboot or kernel. Is it possible to implement such thing?
I think no, I can not find such functionality supported by AM335x GPIO module.
kushal banerjee said:Also, whether a write protect (WP) can be overwritten from JTAG?
AM335x GPIO module has no WP
Regards,
Pavel