This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530 UART2 no work

Other Parts Discussed in Thread: OMAP3530

Hi

I try set UART2 to output  message,but it is not work in X-loader-02.01.03.11.

My UART1 and UART 3 is work.I have add below code in x-loader.Anything is my this attention?

-----------------------------------------------------------------------------------------------------------------

void per_clocks_enable(void)
{
 /* Enable GP2 timer. */
 sr32(CM_CLKSEL_PER, 0, 1, 0x1); /* GPT2 = sys clk */
 sr32(CM_ICLKEN_PER, 3, 1, 0x1); /* ICKen GPT2 */
 sr32(CM_FCLKEN_PER, 3, 1, 0x1); /* FCKen GPT2 */

#ifdef CFG_NS16550
 /* Enable UART1 clocks */
 sr32(CM_FCLKEN1_CORE, 13, 1, 0x1);
 sr32(CM_ICLKEN1_CORE, 13, 1, 0x1);
 /* Enable UART2 clocks */
 sr32(CM_FCLKEN1_CORE, 14, 1, 0x1);
 sr32(CM_ICLKEN1_CORE, 14, 1, 0x1);   
#endif
 delay(1000);
}