Part Number: AM5718
Hi,
Can 4K 30fps image capture be possible with each interface?
① vip
② csi2
Best Regards,
Shigehiro Tsuda
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM5718
Hi,
Can 4K 30fps image capture be possible with each interface?
① vip
② csi2
Best Regards,
Shigehiro Tsuda
Hi RonB,
Thank you for quick reply.
I understand that the answer will be delayed.
It is the information necessary for AM57xx device proposal to our customers.
Please answer as soon as possible.
Best Regards,
Shigehiro Tsuda
Hi Manisha,
Thank you for your reply and detailed explanation.
I can't understand why it can't capture with vip.
The HW limitation of Linux Core VIP User 's Guide has the following description.
Maximum capture width when not using scaling is 8K bytes.
This translates to maximum frame width of - 4K when capturing in YUV 422 mode (2 bytes / pixel)
In the specification of YUV 422, it seems that there is no problem with horizontal size 4 K.
Calculating with the formula described below, it seems that it meets since it is larger than 30 fps.
What's the maximum frame rate possible for W * H resolution using VIP?
FPS = 120 * 1000000 * 2 / (3840 * 2160 * 2) = 31.928
Please tell me why you decided that 4K @ 30fps can not be capture without using multiple ports.
Best Regards,
Shigehiro Tsuda
Hi Shigehiro-San,
Yes, if you use 16-bit bus width with pixel size as 2 bytes per pixel, 4K @30 FPS is possible using VIP interface too. Sorry, I overlooked the bus width in my earlier calculations.
Regards,
Manisha
Hi Manisha,
Thank you for quick reply.
I understood that 4k@30fps capture is possible with vip and csi2.
Best Regards,
Shigehiro Tsuda