Hi !
I have some questions about configuration of DDR Memory.. We developed a board similar to the EVM6437 from Spectrum Digital.. Talking about DDR Memory, we had to change the part number of it because the one that is used by Spectrum was obsolete.. There are some differences in the memory... The principal ones are:
EVM (MT47H32M16CC-37E Supplied by Micron) - It has 8Megx16x4Banks, works with CK3,75ns, CL=4 - DDR2-533
Our board (MT47H64M16HR-3:E supplied by Micron) - It has 8Megx16x8Banks, works with CK3ns, CL=4 - DDR2-667
My question is..Where and How I change it on DM6437 Demo Software(Supplied with EVM6437) ?? May I supposed to change the PLL2 Configuration?? How did I do it?
In evmdm6437.c source file there was the command "EVMDM6437_enable Pll2 ( 0 , 23 , 11 , 1) */Vpss @ 54MHz / DDR @ 162MHz */"
I didn´t understand what it means, and how can I modify it because by the part number my DDR memory works at 533MHz
Please, if somebody could help me to understand it..
Best Regards
Denis Kenji Kimura