Other Parts Discussed in Thread: SN65HVD75
Tool/software: Linux
We are using UART 4 and 5 connected to RS485 transceivers and have connected the Tx/RX control lines to their respective RTS signals from the UARTs.
Everything is working as expected when the application is running, however during boot up the RTS lines default to '1' and this enables the RS485 transmitters. I understand why this is happening but I am somewhat stumped as what to do about it.
So my question is what solutions are there to get the system to boot with the RTS lines low until the RS485 mode of the serial driver needs to use them?
Thanks
Ty