hi,
i'm use of DM6467. on the EDMA3, i want to link some 3-dimension DMA, but CAN NOT! why?
this is the cfg:
// config param
chanParam->OPT = CSL_EDMA_OPT_MAKE(
CSL_EDMACC_OPT_ITCCHEN_ENABLE,
CSL_EDMACC_OPT_TCCHEN_DISABLE,
CSL_EDMACC_OPT_ITCINTEN_DISABLE,
CSL_EDMACC_OPT_TCINTEN_ENABLE,
tcc,
CSL_EDMACC_OPT_TCCMODE_NORMAL,
CSL_EDMACC_OPT_FWID_8,
CSL_EDMACC_OPT_STATIC_NORMAL,
CSL_EDMACC_OPT_SYNCDIM_ABSYNC,
CSL_EDMACC_OPT_DAM_INCR,
CSL_EDMACC_OPT_SAM_INCR
);
chanParam->SRC = (Uint32)src;
chanParam->A_B_CNT = (numLines<<16)| numBytes;
chanParam->DST = (Uint32)dst;
chanParam->SRC_DST_BIDX = (dstPitch<<16)|srcPitch;
chanParam->LINK_BCNTRLD = (0x1<<16)|0x4020;
chanParam->SRC_DST_CIDX = (dst_cIdx<<16)|src_cIdx;
chanParam->CCNT = ccnt;
if somebody could tell, I'll be very grateful.