This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/OMAP-L138: Need exact version of SYS-BIOS/RTOS to run on the OMAP-L138

Part Number: OMAP-L138


Tool/software: TI-RTOS

This is my first project with OMAP-L138. I've installed CCS v8.2 and was about to download RTOS.

I'm having real problems with finding it under App Center. It's recommended to install it via App Center. 

I've been reading related manuals and in conclusion , I seems that I need older version of SYS-BIOS. 

The question now for me is which SYS-BIOS version do I need? Or RTOS is till OK?  If so, which one do I need? 

Thank you in advance for your help in finding an answer,

Jacek