Hello,
What is the safe way of using PWM in driving stepper motors?
Can we directly connect PWM pins to wires on the stepper motor? In this case, voltage difference between PWM pins will directly be applied to wire ends of the stepper motor, hence the current flowing throught the motor will also flow through the internal of the chip, entering at one PWM and comes out from another. If the current is large, is it possible for the chip to get burned?
If this is a limitation on the amplitude of the current, does this mean that we can only use PWM to motors with very small power (hence current)? Then are PWMs still good for any practical use?
Could anyone explain these to me?
Garry