Other Parts Discussed in Thread: TPS65217
Tool/software: Linux
Hi all,
I am experiencing issues with the device tree setup of the AR1021 Resistive Touch Controller. It seems that the driver is detecting the controller and attaching it to its address correctly but, I am having issues configuring the interrupt pin and I am getting the following from my boot log:
[ 3.636603] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 5.653150] pinctrl-single 44e10800.pinmux: mux offset out of range: 0xfffff99c (0x)
[ 5.661278] pinctrl-single 44e10800.pinmux: could not add functions for ar1021_pinsx
Device Tree:
&i2c0 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&i2c0_pins>;
// configuration start
clock-frequency = <100000>;
#address-cells = <1>;
#size-cells = <0>;
ar1021_i2c: ar1021_i2c@4d {
#address-cells = <1>;
#size-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&ar1021_pins>;
compatible = "microchip,ar1021-i2c";
reg = <0x4d>;
interrupt-parent = <&gpio3>;
interrupts = <17 IRQ_TYPE_LEVEL_HIGH>;
touchscreen-offset-x=<250>;
touchscreen-offset-y=<300>;
touchscreen-inverted-y;
};
};
&am33xx_pinmux {
ar1021_pins: ar1021_pins {
pinctrl-single,pins = <
AM33XX_IOPAD(0x19c, PIN_INPUT | MUX_MODE7) /* (C12) mcasp0_ahclkr.gpio3[17] */
>;
};
Kernel Version: 4.9.119-bone11
Complete Boot Log:
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.9.119-bone11 (root@oscar-ideacentre-300S-08IHH) (gcc ve8
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt:Machine model: TI AM335x BeagleBone Black
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x9d000000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] On node 0 totalpages: 131072
[ 0.000000] free_area_init_node: node 0, pgdat c13d5194, node_mem_map dcb61000
[ 0.000000] Normal zone: 1152 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 131072 pages, LIFO batch:31
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 120
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p1 ro roott
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 449572K/524288K available (12288K kernel code, 1059K rwdata, 40)
[ 0.000000] Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xe0800000 - 0xff800000 ( 496 MB)
lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0xc0008000 - 0xc0d00000 (13280 kB)
.init : 0xc1200000 - 0xc1300000 (1024 kB)
.data : 0xc1300000 - 0xc1408d1c (1060 kB)
.bss : 0xc140a000 - 0xc14b4490 ( 682 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000016] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971s
[ 0.000038] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_s
[ 0.000050] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000569] clocksource_probe: no matching clocksources found
[ 0.000750] Console: colour dummy device 80x30
[ 0.000777] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000784] This ensures that you still see kernel messages. Please
[ 0.000791] update your kernel commandline.
[ 0.000813] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.088884] pid_max: default: 32768 minimum: 301
[ 0.089134] Security Framework initialized
[ 0.089147] Yama: becoming mindful.
[ 0.089183] AppArmor: AppArmor disabled by boot time parameter
[ 0.089378] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089391] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.090404] CPU: Testing write buffer coherency: ok
[ 0.090469] ftrace: allocating 37499 entries in 110 pages
[ 0.196449] Setting up static identity map for 0x80100000 - 0x80100058
[ 0.199913] EFI services will not be available.
[ 0.201580] devtmpfs: initialized
[ 0.216946] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.217391] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idles
[ 0.217417] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.221075] xor: measuring software checksum speed
[ 0.318913] arm4regs : 1220.000 MB/sec
[ 0.418855] 8regs : 958.000 MB/sec
[ 0.518843] 32regs : 1090.400 MB/sec
[ 0.618843] neon : 1666.800 MB/sec
[ 0.618852] xor: using function: neon (1666.800 MB/sec)
[ 0.618872] pinctrl core: initialized pinctrl subsystem
[ 0.620180] NET: Registered protocol family 16
[ 0.622425] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.639275] omap_hwmod: debugss: _wait_target_disable failed
[ 0.708870] cpuidle: using governor menu
[ 0.715121] OMAP GPIO hardware version 0.1
[ 0.731489] No ATAGs?
[ 0.731516] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.938990] raid6: int32x1 gen() 251 MB/s
[ 1.108904] raid6: int32x1 xor() 218 MB/s
[ 1.279012] raid6: int32x2 gen() 327 MB/s
[ 1.448865] raid6: int32x2 xor() 265 MB/s
[ 1.618912] raid6: int32x4 gen() 306 MB/s
[ 1.788889] raid6: int32x4 xor() 246 MB/s
[ 1.958843] raid6: int32x8 gen() 295 MB/s
[ 2.128852] raid6: int32x8 xor() 210 MB/s
[ 2.298877] raid6: neonx1 gen() 1455 MB/s
[ 2.468853] raid6: neonx1 xor() 845 MB/s
[ 2.618839] random: fast init done
[ 2.638862] raid6: neonx2 gen() 1919 MB/s
[ 2.808842] raid6: neonx2 xor() 1195 MB/s
[ 2.978863] raid6: neonx4 gen() 1955 MB/s
[ 3.148854] raid6: neonx4 xor() 1210 MB/s
[ 3.318873] raid6: neonx8 gen() 1097 MB/s
[ 3.488842] raid6: neonx8 xor() 782 MB/s
[ 3.488850] raid6: using algorithm neonx4 gen() 1955 MB/s
[ 3.488857] raid6: .... xor() 1210 MB/s, rmw enabled
[ 3.488864] raid6: using intx1 recovery algorithm
[ 3.496669] edma 49000000.edma: TI EDMA DMA engine driver
[ 3.498992] SCSI subsystem initialized
[ 3.499353] libata version 3.00 loaded.
[ 3.499675] usbcore: registered new interface driver usbfs
[ 3.499746] usbcore: registered new interface driver hub
[ 3.499841] usbcore: registered new device driver usb
[ 3.500353] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44ce
[ 3.500403] omap_i2c 4819c000.i2c: could not find pctldev for node /ocp/l4_wkup@44ce
[ 3.500512] media: Linux media interface: v0.10
[ 3.500566] Linux video capture interface: v2.00
[ 3.500641] pps_core: LinuxPPS API ver. 1 registered
[ 3.500649] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <g>
[ 3.500671] PTP clock support registered
[ 3.501169] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 3.501812] Advanced Linux Sound Architecture Driver Initialized.
[ 3.503072] NetLabel: Initializing
[ 3.503087] NetLabel: domain hash size = 128
[ 3.503092] NetLabel: protocols = UNLABELED CIPSOv4
[ 3.503174] NetLabel: unlabeled traffic allowed by default
[ 3.503840] clocksource: Switched to clocksource timer1
[ 3.594025] VFS: Disk quotas dquot_6.6.0
[ 3.594124] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 3.605912] NET: Registered protocol family 2
[ 3.606680] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 3.606726] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 3.606765] TCP: Hash tables configured (established 4096 bind 4096)
[ 3.606836] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 3.606854] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 3.607002] NET: Registered protocol family 1
[ 3.607591] RPC: Registered named UNIX socket transport module.
[ 3.607605] RPC: Registered udp transport module.
[ 3.607611] RPC: Registered tcp transport module.
[ 3.607618] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 3.608343] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters avaie
[ 3.610533] audit: initializing netlink subsys (disabled)
[ 3.610630] audit: type=2000 audit(3.540:1): initialized
[ 3.611665] workingset: timestamp_bits=14 max_order=17 bucket_order=3
[ 3.620725] zbud: loaded
[ 3.624412] NFS: Registering the id_resolver key type
[ 3.624465] Key type id_resolver registered
[ 3.624474] Key type id_legacy registered
[ 3.624493] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 3.624815] fuse init (API version 7.26)
[ 3.625748] orangefs_debugfs_init: called with debug mask: :none: :0:
[ 3.625991] orangefs_init: module version upstream loaded
[ 3.626002] SGI XFS with ACLs, security attributes, realtime, no debug enabled
[ 3.634677] Key type asymmetric registered
[ 3.634700] Asymmetric key parser 'x509' registered
[ 3.635034] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 3.635250] io scheduler noop registered
[ 3.635262] io scheduler deadline registered
[ 3.635519] io scheduler cfq registered (default)
[ 3.636603] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 3.638907] backlight supply power not found, using dummy regulator
[ 3.640378] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 3.641396] Serial: 8250/16550 driver, 6 ports, IRQ sharing disabled
[ 3.644059] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 300000
[ 4.475779] console [ttyS0] enabled
[ 4.481332] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ 4.488286] [drm] Initialized
[ 4.493180] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 4.499971] [drm] No driver support for vblank timestamp query.
[ 4.563874] ------------[ cut here ]------------
[ 4.563918] WARNING: CPU: 0 PID: 1 at drivers/gpu/drm/drm_atomic_helper.c:1140 drm_c
[ 4.563922] [CRTC:24] vblank wait timed out
[ 4.563930] Modules linked in:
[ 4.563941] CPU: 0 PID: 1 Comm: swapper Not tainted 4.9.119-bone11 #18
[ 4.563944] Hardware name: Generic AM33XX (Flattened Device Tree)
[ 4.563980] [<c0110e50>] (unwind_backtrace) from [<c010d7b4>] (show_stack+0x20/0x24)
[ 4.563996] [<c010d7b4>] (show_stack) from [<c06efd34>] (dump_stack+0x24/0x28)
[ 4.564019] [<c06efd34>] (dump_stack) from [<c0135930>] (__warn+0xf4/0x10c)
[ 4.564031] [<c0135930>] (__warn) from [<c013599c>] (warn_slowpath_fmt+0x54/0x70)
[ 4.564044] [<c013599c>] (warn_slowpath_fmt) from [<c07d5f88>] (drm_atomic_helper_w)
[ 4.564067] [<c07d5f88>] (drm_atomic_helper_wait_for_vblanks) from [<c080d89c>] (ti)
[ 4.564083] [<c080d89c>] (tilcdc_commit) from [<c07fab08>] (drm_atomic_commit+0x5c/)
[ 4.564098] [<c07fab08>] (drm_atomic_commit) from [<c07dc208>] (restore_fbdev_mode+)
[ 4.564110] [<c07dc208>] (restore_fbdev_mode) from [<c07dd2dc>] (drm_fb_helper_rest)
[ 4.564120] [<c07dd2dc>] (drm_fb_helper_restore_fbdev_mode_unlocked) from [<c07dd36)
[ 4.564132] [<c07dd364>] (drm_fb_helper_set_par) from [<c074b2ec>] (fbcon_init+0x4f)
[ 4.564151] [<c074b2ec>] (fbcon_init) from [<c07a4794>] (visual_init+0xcc/0x110)
[ 4.564163] [<c07a4794>] (visual_init) from [<c07a5dfc>] (do_bind_con_driver+0x1bc/)
[ 4.564174] [<c07a5dfc>] (do_bind_con_driver) from [<c07a63dc>] (do_take_over_conso)
[ 4.564183] [<c07a63dc>] (do_take_over_console) from [<c074b3bc>] (do_fbcon_takeove)
[ 4.564193] [<c074b3bc>] (do_fbcon_takeover) from [<c074eec0>] (fbcon_event_notify+)
[ 4.564212] [<c074eec0>] (fbcon_event_notify) from [<c01599c0>] (notifier_call_chai)
[ 4.564224] [<c01599c0>] (notifier_call_chain) from [<c0159ec0>] (__blocking_notifi)
[ 4.564235] [<c0159ec0>] (__blocking_notifier_call_chain) from [<c0159f00>] (blocki)
[ 4.564249] [<c0159f00>] (blocking_notifier_call_chain) from [<c07551c8>] (fb_notif)
[ 4.564260] [<c07551c8>] (fb_notifier_call_chain) from [<c07572b4>] (register_frame)
[ 4.564271] [<c07572b4>] (register_framebuffer) from [<c07dd660>] (drm_fb_helper_in)
[ 4.564281] [<c07dd660>] (drm_fb_helper_initial_config) from [<c07de01c>] (drm_fbde)
[ 4.564290] [<c07de01c>] (drm_fbdev_cma_init_with_funcs) from [<c07de0bc>] (drm_fbd)
[ 4.564301] [<c07de0bc>] (drm_fbdev_cma_init) from [<c080d788>] (tilcdc_load+0x62c/)
[ 4.564310] [<c080d788>] (tilcdc_load) from [<c07e8534>] (drm_dev_register+0xc0/0xe)
[ 4.564321] [<c07e8534>] (drm_dev_register) from [<c07e9ba8>] (drm_platform_init+0x)
[ 4.564331] [<c07e9ba8>] (drm_platform_init) from [<c080d998>] (tilcdc_pdev_probe+0)
[ 4.564351] [<c080d998>] (tilcdc_pdev_probe) from [<c081b958>] (platform_drv_probe+)
[ 4.564363] [<c081b958>] (platform_drv_probe) from [<c08193e4>] (driver_probe_devic)
[ 4.564373] [<c08193e4>] (driver_probe_device) from [<c081980c>] (__driver_attach+0)
[ 4.564383] [<c081980c>] (__driver_attach) from [<c0816f40>] (bus_for_each_dev+0x8c)
[ 4.564393] [<c0816f40>] (bus_for_each_dev) from [<c0818c10>] (driver_attach+0x2c/0)
[ 4.564403] [<c0818c10>] (driver_attach) from [<c0818644>] (bus_add_driver+0x16c/0x)
[ 4.564413] [<c0818644>] (bus_add_driver) from [<c081a3ac>] (driver_register+0x88/0)
[ 4.564423] [<c081a3ac>] (driver_register) from [<c081b8a4>] (__platform_driver_reg)
[ 4.564443] [<c081b8a4>] (__platform_driver_register) from [<c124a9f0>] (tilcdc_drm)
[ 4.564456] [<c124a9f0>] (tilcdc_drm_init) from [<c0101b8c>] (do_one_initcall+0x68/)
[ 4.564476] [<c0101b8c>] (do_one_initcall) from [<c1200fc0>] (kernel_init_freeable+)
[ 4.564500] [<c1200fc0>] (kernel_init_freeable) from [<c0cae454>] (kernel_init+0x18)
[ 4.564517] [<c0cae454>] (kernel_init) from [<c0108f10>] (ret_from_fork+0x14/0x24)
[ 4.564532] ---[ end trace 10cfcc05a75e1efb ]---
[ 4.573932] Console: switching to colour frame buffer device 240x45
[ 4.988690] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 5.023878] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[ 5.033522] libphy: Fixed MDIO Bus: probed
[ 5.103928] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 5.110136] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[ 5.116757] davinci_mdio: dt: updated phy_id[0] from phy_mask[fffffffe]
[ 5.124559] libphy: 4a101000.mdio: probed
[ 5.128610] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMS0
[ 5.138598] cpsw 4a100000.ethernet: Detected MACID = c8:fd:19:c5:e4:a8
[ 5.147125] usbcore: registered new interface driver usb-storage
[ 5.155163] 47401300.usb-phy supply vcc not found, using dummy regulator
[ 5.166762] 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 5.176938] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[ 5.182848] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number1
[ 5.191018] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 5.197873] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 5.205144] usb usb1: Product: MUSB HDRC host driver
[ 5.210142] usb usb1: Manufacturer: Linux 4.9.119-bone11 musb-hcd
[ 5.216278] usb usb1: SerialNumber: musb-hdrc.1.auto
[ 5.222090] hub 1-0:1.0: USB hub found
[ 5.226091] hub 1-0:1.0: 1 port detected
[ 5.240430] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[ 5.248633] i2c /dev entries driver
[ 5.254153] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 5.261506] softdog: initialized. soft_noboot=0 soft_margin=60 sec soft_panic=0 (no)
[ 5.271338] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 5.395092] ledtrig-cpu: registered to indicate activity on CPUs
[ 5.401436] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 5.407789] omap-aes 53500000.aes: will run requests pump with realtime priority
[ 5.419730] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 5.427272] hidraw: raw HID events driver (C) Jiri Kosina
[ 5.433516] usbcore: registered new interface driver usbhid
[ 5.439277] usbhid: USB HID core driver
[ 5.443497] remoteproc0: wkup_m3 is available
[ 5.449223] remoteproc0: Note: remoteproc is still under development and considere.
[ 5.458387] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward comp.
[ 5.472523] wireguard: WireGuard 0.0.20180809 loaded. See www.wireguard.com for inf.
[ 5.481357] wireguard: Copyright (C) 2015-2018 Jason A. Donenfeld <Jason@zx2c4.com>.
[ 5.492052] NET: Registered protocol family 10
[ 5.497945] mip6: Mobile IPv6
[ 5.501010] mmc0: host does not support reading read-only switch, assuming write-ene
[ 5.509290] mmc0: new high speed SDHC card at address aaaa
[ 5.510108] mmcblk0: mmc0:aaaa SL16G 14.8 GiB
[ 5.516716] mmcblk0: p1
[ 5.524772] NET: Registered protocol family 17
[ 5.529364] Key type dns_resolver registered
[ 5.533654] mpls_gso: MPLS GSO support
[ 5.537705] omap_voltage_late_init: Voltage driver support not added
[ 5.544358] ThumbEE CPU extension supported.
[ 5.548663] Registering SWP/SWPB emulation handler
[ 5.554499] registered taskstats version 1
[ 5.558749] zswap: loaded using pool lzo/zbud
[ 5.565800] Btrfs loaded, crc32c=crc32c-generic
[ 5.571954] Key type encrypted registered
[ 5.627619] input: tps65217_pwr_but as /devices/platform/ocp/44e0b000.i2c/i2c-0/0-00
[ 5.640194] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 5.646052] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 5.653150] pinctrl-single 44e10800.pinmux: mux offset out of range: 0xfffff99c (0x)
[ 5.661278] pinctrl-single 44e10800.pinmux: could not add functions for ar1021_pinsx
[ 5.670781] input: ar1021 I2C Touchscreen as /devices/platform/ocp/44e0b000.i2c/i2c1
[ 5.680813] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 100 kHz
[ 5.687941] at24 2-0054: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 5.695249] at24 2-0055: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 5.702516] at24 2-0056: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 5.709761] at24 2-0057: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 5.716751] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz
[ 5.723202] remoteproc0: powering up wkup_m3
[ 5.727692] remoteproc0: Booting fw image am335x-pm-firmware.elf, size 217168
[ 5.735380] remoteproc0: remote processor wkup_m3 is now up
[ 5.741079] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x193
[ 5.762895] bone_capemgr bone_capemgr: Baseboard: 'A335BNLT,000C,1823BBBG0042'
[ 5.770235] bone_capemgr bone_capemgr: compatible-baseboard=ti,beaglebone-black - #4
[ 5.805522] bone_capemgr bone_capemgr: slot #0: No cape found
[ 5.834406] bone_capemgr bone_capemgr: slot #1: No cape found
[ 5.864925] bone_capemgr bone_capemgr: slot #2: No cape found
[ 5.895456] bone_capemgr bone_capemgr: slot #3: No cape found
[ 5.901294] bone_capemgr bone_capemgr: initialized OK.
[ 5.909379] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01 00:00:01 UTC )
[ 5.918205] of_cfs_init
[ 5.920771] of_cfs_init: OK
[ 5.924198] PM: Hibernation image not present or could not be loaded.
[ 5.924320] ALSA device list:
[ 5.927396] No soundcards found.
[ 5.946240] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Opts: ()
[ 5.954588] VFS: Mounted root (ext4 filesystem) readonly on device 179:1.
[ 5.967283] devtmpfs: mounted
[ 5.971629] Freeing unused kernel memory: 1024K
[ 6.373085] systemd[1]: System time before build time, advancing clock.
[ 6.442897] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 6.464286] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.474078] random: systemd: uninitialized urandom read (16 bytes read)
[ 6.492926] systemd[1]: systemd 232 running in system mode. (+PAM +AUDIT +SELINUX +)
[ 6.511934] systemd[1]: Detected architecture arm.
[ 6.548138] systemd[1]: Set hostname to <arm>.
[ 6.713052] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read)
[ 7.130761] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ 7.175499] systemd[1]: Created slice System Slice.
[ 7.204608] systemd[1]: Listening on Journal Socket (/dev/log).
[ 7.234596] systemd[1]: Listening on udev Control Socket.
[ 7.265188] systemd[1]: Created slice User and Session Slice.
[ 7.294182] systemd[1]: Reached target Slices.
[ 7.325169] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ 8.407055] EXT4-fs (mmcblk0p1): re-mounted. Opts: errors=remount-ro
[ 8.983665] systemd-journald[125]: Received request to flush runtime journal from P1
[ 10.644487] net eth0: initializing cpsw version 1.12 (0)
[ 10.774692] SMSC LAN8710/LAN8720 4a101000.mdio:00: attached PHY driver [SMSC LAN871)
[ 10.889430] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 12.094078] nf_conntrack version 0.5.0 (8192 buckets, 32768 max)
[ 12.366571] Bluetooth: Core ver 2.22
[ 12.383745] NET: Registered protocol family 31
[ 12.416293] Bluetooth: HCI device and connection manager initialized
[ 12.451888] Bluetooth: HCI socket layer initialized
[ 12.479412] Bluetooth: L2CAP socket layer initialized
[ 12.507457] Bluetooth: SCO socket layer initialized
[ 12.944758] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx
[ 12.990538] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 13.170354] 8021q: 802.1Q VLAN Support v1.8
[ 13.204225] 8021q: adding VLAN 0 to HW filter on device eth0
[ 14.126829] using random self ethernet address
[ 14.131323] using random host ethernet address
[ 14.179288] using random self ethernet address
[ 14.189082] using random host ethernet address
[ 14.300327] usb0: HOST MAC c8:fd:19:c5:e4:a9
[ 14.315211] usb0: MAC c8:fd:19:c5:e4:aa
[ 14.334839] usb1: HOST MAC c8:fd:19:c5:e4:ac
[ 14.359540] usb1: MAC c8:fd:19:c5:e4:ad
[ 14.764055] configfs-gadget gadget: high-speed config #1: c
[ 14.923367] IPv6: ADDRCONF(NETDEV_UP): usb1: link is not ready
[ 18.039376] CAN device driver interface
[ 18.324426] c_can_platform 481d0000.can: c_can_platform device registered (regs=fa1)
[ 171.304854] sysrq: SysRq : HELP : loglevel(0-9) reboot(b) crash(c) terminate-all-ta
[ 174.482388] sysrq: SysRq : HELP : loglevel(0-9) reboot(b) crash(c) terminate-all-ta
[ 177.482267] sysrq: SysRq : HELP : loglevel(0-9) reboot(b) crash(c) terminate-all-ta
[ 294.390263] random: crng init done
[ 294.393753] random: 7 urandom warning(s) missed due to ratelimiting
I have tried a few different methods to configure the interrupt pin with the same result. Any help would be greatly appreciated.
Regards,
Oscar