Part Number: AM6548
Tool/software: Linux
Hi TI,
I encountered the following error when boot from opsi flash(MMC0), So I can't access SD card(MMC1).
MMC: sdhci@0: 0, sdhci@0: 1
sdhci_send_command: MMC: 1 busy timeout increasing to: 200 ms.
sdhci_send_command: MMC: 1 busy timeout increasing to: 400 ms.
sdhci_send_command: MMC: 1 busy timeout increasing to: 800 ms.
sdhci_send_command: MMC: 1 busy timeout increasing to: 1600 ms.
sdhci_send_command: MMC: 1 busy timeout increasing to: 3200 ms.
sdhci_send_command: MMC: 1 busy timeout.
But it can work when I booted from SD card. Under this conditions, MMC0 and MMC1 both work good.
My setup:
AM6548 EVM board
Processor SDK 05_01_00_11
Thanks
BS