This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: How to set my cpu to maximum speed

Part Number: AM5728

Hello,

1) We are using SDK TI-SDK-4.0.0.4-kernel-4.9.28 and want to set the CPU frequency to 1.5GHz without frequency scaling.

Could you please let us know the step by step procedure to do this?

2) We want to look at the current cpu frequency and understand there are many ways to this.

- sysfs is not an option as we don't have freq scaling enabled and I only see

root@CPS:/sys/devices/system/cpu/cpu0# ls
of_node    power      subsystem  topology   uevent

- cat /proc/cpuinfo shows


root@CPS:/sys/devices/system/cpu/cpufreq# cat /proc/cpuinfo
processor       : 0
model name      : ARMv7 Processor rev 2 (v7l)
BogoMIPS        : 12.29
Features        : half thumb fastmult vfp edsp neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae evtstrm
CPU implementer : 0x41
CPU architecture: 7
CPU variant     : 0x2
CPU part        : 0xc0f
CPU revision    : 2

I don't see the CPU frequency but there is a BogoMips field which seemed to be a low value(12.29). Is this correct?

Thanks,

Swapna