This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CPU Load Graph Questions

Guru 15580 points


I recently upgraded to CCS4.2 and have the following questions regarding the CPU load graph.

1. When the CPU Load graph is first started it comes up with no grids and no background color. If I change these settings they do appear in the currently running graph, but they do not "stick". In otherwords, if I stop the debug session and restart it, the CPU Load graph comes up with no background color and no grid lines. I have also tried saving the perspective with these settings set but it does not help.

2. Autoscale seems to work, but I can't reverse it. (rest auto scale).

3. The RTA time unit always comes up in "time" but shows "ticks".

Can someone help me with a resolution to these issues?

thx

MikeH