On a custom DM355 board, cmem does not create a device node. insmod command was taken from loadmodules.sh (part of dvsdk demo).
| root@custombrd:/media/card# insmod cmemk.ko phys_start=0x86000000 phys_end=0x88000 000 pools=10x829440,1x1529856,1x276,1x4320,1x560,2x344,1x144,1x81920,2x512,1x140 00,1x12960,1x11360,1x4,2x296,1x8192,59x56,4x24,1x1505280,9x1658880,1x2258880CMEM K module: built on Nov 18 2010 at 12:37:59 Reference Linux version 2.6.32 File /home/vmplanet/dvsdk/dvsdk_3_10_00_19/linuxutils_2_25_04_10/packages/ti/s do/linuxutils/cmem/src/module/cmemk.c allocated heap buffer 0xca000000 of size 0x45b000 cmemk initialized root@custombrd:/media/card# ls /dev/ apm_bios hda hda2 mmcblk0p1 mtd5 ptmx tty4 console hda1 hda3 mmcblk0p2 mtd6 pts tty5 dm350mmap hda10 hda4 mmcblk0p3 mtd7 ram0 tty6 event0 hda11 hda5 mmcblk0p4 mtdblock0 ram1 tty7 event1 hda12 hda6 mmcblk0p5 mtdblock1 ram2 tty8 event2 hda13 hda7 mmcblk0p6 mtdblock2 ram3 ttyS0 event3 hda14 hda8 mmcblk0p7 mtdblock3 random ttySA0 event4 hda15 hda9 mtd0 mtdblock4 tty urandom event5 hda16 initctl mtd1 mtdblock5 tty0 zero event6 hda17 kmem mtd2 mtdblock6 tty1 event7 hda18 mem mtd3 mtdblock7 tty2 fb0 hda19 mmcblk0 mtd4 null tty3 root@custombrd:/media/card# |
What could be the problem?