hai,
1)i am using am5728 GP EVM, i am trying to pick a dedicated GPIO pin among the available GPIO pins(which are divided into 8 GPIO banks) in AM5728, but i am unable to know which is the unused GPIO pin ( no other modes connected to that GPIO pin). So, that there will be no pin conflicts when that such GPIO pin is used.
2)i am unable to know which GPIO banks are enabled in SDK i use (ti-processor-sdk-linux-am57xx-evm-05.00.00.15).
can u help me to solve the above problems.