I am using AM3517EVM with PSP03.00.01.06 package. Both x-loader and u-boot are configured with default
configurations. The board boots to u-boot console normally. Then I can ping to other PCs from u-boot.
However, after 30-60 minutes idle state of u-boot, I try to use 'ping' again. The board hangs at 'ping' command.
Is there time out setting in u-boot code for ethernet?