Part Number: TMDXIDK437X
Hello,
I have two questions related to TIDEP0025.
1, From the document, it seems to be nesessary to download EtherCAT slave stack and access the source file.
If we are not ETG member, Are there any information how to run TIDEP0025 demo(Endat 2.2)?
2, I would like to run TIDEP0025 demo using tamagawa encoder also.
Is there any other necessary parts other than the following?
· CPU evaluation board: TMDSIDK 437x
· RS485 interface board: RS485-HF-DPLX-EVM
· BLDC motor: BLY 171 D - 24 V - 4000 / Anaheim Automation
· Tamagawa encoder: TS 5667 N 320 / Tamagawa Seiki Co., Ltd.
Regards,
U-SK