This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM644X Internal Pullup/Pulldown (IPU/IPD) state on EMIF configuration pins during reset

In looking at the DM6446 REV-F datasheet, I am confused if certain terminal pins have internal pullups or pulldowns. I am attempting to minimize logic required to configure the board in reset.

Specifically,  The AEAW(YOUT4-0) and COUT(COUT3-0) pins have IPD internal pulldowns documented in Table 2-5 (page 27) and Table 2-9 (page 29),  and are also shown as part of the "low-group" in Figure 6-9 on page 102. Yet, in that same figure 6-9, they are documented as being in the "Z-group" with IPU internal pullUPS.  How can they be in both "low" and "Z" groups?

Do they have internal pullups or pulldowns? Does that change during reset?

I am not quite sure how to read this.

- Gary