Is there a way to configure the C5515 timers to stop when the processor is halted in CCS? This is possible with some of the other C5000 devices via FREE/SOFT bits, but I didn't see anything like this in the C5515 timer usersguide.
-Ruben
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a way to configure the C5515 timers to stop when the processor is halted in CCS? This is possible with some of the other C5000 devices via FREE/SOFT bits, but I didn't see anything like this in the C5515 timer usersguide.
-Ruben
Ruben,
No, the C5515 does not have that capability.
Regards,
Peter Chung