Hi All
I would like to know the status of IR SDOCM00069806 in AM35x-OMAP35x-PSP_03.00.01.06_Release_Notes:
|
SDOCM00069806 |
Video Display: GFX FIFO underflow observed when using DSS with higher resolution + VRFB rotation |
My customer wants to implement the screen/video rotation feature with a high resolution LCD screen (1366*768). Is it possible to implement 90,180,270 rotations during video playing with VRFB/DMA method which should cause huge bandwidth consumption? Or we can only implement it in application layer?
If yes, how about the performance? If no, do you know the maximum resolution limitation to implement this function?
Thanks a lot for your help!