This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2EVM5777: DDR Configurations for VisionSDK Linux

Part Number: TDA2EVM5777

Tool/software: Linux

Hello,

I am running PROCESSOR_SDK_VISION_03_03_00_00 on the TDA2EVM5777 and on custom hardware that is similar to the EVM. I can successfully boot on the new hardware with the default memory that comes with Vision SDK (note there is nothing on our custom hardware's EEPROM at this time). I need to update Linux in order to utilize the 4GB of ram on the custom hardware setup, instead of default settings.

Can you please help clarify exactly what is required to allow me to use all 4GB of ram on the custom hardware? Below is what I tried/my assumptions

1. Since the custom hardware does not contain any firmware for EEPROM, and is able to boot OK, I assume its using the default settings from the u-boot source just fine, however, the Linux user space only sees 600MB of ram total (found by running the command free) where there is supposed to be 1.5GB in default settings I believe, based on dra7-evm.dts file below settings:

memory {
device_type = "memory";
reg = <0x0 0x80000000 0x0 0x60000000>; /* 1536 MB */
};


How do I get access to more memory in user space with the default settings?


2. Since the custom hardware actually contains 4GB DDR, I want to change the bootloader to recognize the ram modules that I have, and so I followed this document. In the document, I was able to successfully use the EMIF configuration tool to generate the values necessary to update the u-boot source codes. When I finished filling out the EMIF configuration tool it generated LISA map register values to update evm.c with (the values for each LISA map register were very similar to the example for 2GB per EMIF settings given in evm.c). However, I haven't been able to successfully boot up using the updated source files yet. I didn't update the dra7-evm.dts to be 4GB yet, but unsure if that is the cause why it didn't boot. I didn't change anything in EEPROM either, since I have never had anything written to EEPROM and hoping I can just modify the default settings to be 4GB.


Can you please help clarify exactly what is required to allow me to use all 4GB of ram on the custom hardware without writing to EEPROM?

Thank you in advance,
-iFer