This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA76P: DDR3 configuration for 4GB

Part Number: DRA76P


Tool/software: Linux

Hi All,

I am using PSDK 3.03 having U-boot 2016 and a custom board is having 4GB RAM

Currently the EVM board has 1.5GB RAM. I need to configure it 4GB .

We have EMIF1 part number  MT41K512M16HA-125 * 2-----------(2GB) with ECC

And EMIF2 part number MT41K512M8DA-107  * 4 ----------------------(2GB)

I have read the document   

 CONFIG_ARMV7_LPAE = y is enabled in the defconfig

Also I have changed the LISA MAP to 

static const struct dmm_lisa_map_regs lisa_map_dra7_4Gb = {
.dmm_lisa_map_0 = 0x0,
.dmm_lisa_map_1 = 0x0,
.dmm_lisa_map_2 = 0xx80700100,-------------------(EMIF1 2 GB non interleaved)
.dmm_lisa_map_3 = 0xFF720200,-------------------------- (EMIF1 2 GB non interleaved)
.is_ma_present = 0x1
};

Also I am not sure which LISA_MAP (i.e 0,1,2,3) has to be selected. Can I use any two out of four?

The board is booting with only 2GB

Can anyone help me to configure the EMIF1 and EMIF2 for 4GB memory.

Also what changes are required in the dts files for uboot and kernel.

Thanks

Deep

  • Hi,

    Anyone who can help me on this.
    We are not using interleaving of memory.Is it required?
    Will interleaving work if we are having EMIF1 with ECC?

    Thanks

  • Hi,

    There is a similar thread (link below) which discusses disabling interleaving for high-order memory, as well as the DMM LISA register settings.

    e2e.ti.com/.../686907

    One thing to note is that the LISA registers should only be used to configure the shared DDR memory space (0x8000_0000 - 0xFFFF_FFFF). The high order memory is fixed and accessible by only the MPU. 

    The fixed high-order mapping can not access the lowest 1GB of each EMIF. Thus, the lowest 1 GB on each EMIF needs to be assigned in the DMM.

    As an example, you could set the following for no interleaving:

    static const struct dmm_lisa_map_regs lisa_map_dra7_4Gb = {
    .dmm_lisa_map_0 = 0x0,
    .dmm_lisa_map_1 = 0x80600100,   // (EMIF1: 1 GB non interleaved)
    .dmm_lisa_map_2 = 0xC0600200,  // (EMIF2: 1 GB non interleaved)
    .dmm_lisa_map_3 = 0xFF020100,
    .is_ma_present = 0x1
    };

    The easiest integration with existing u-boot software would be to keep the high order memory interleaved. If this approach is taken, the only other modification you should need is to ensure that the lines of code below are included in the function "dram_init_banksize" inside "/board/ti/dra7xx/evm.c", which declares the extended memory sections. 

    gd->bd->bi_dram[1].start = 0x200000000;
    gd->bd->bi_dram[1].size = 0x80000000;

    If this is not feasible due to ECC, then please let us know.

    Best regards,
    Kevin

  • Hi Kevin,

    Thanks a lot for your reply.

    I will check and let you know.

    Regards,

    Deep

  • Former Member
    0 Former Member in reply to deepikateriar
    Hi,
    Do you have any further updates on this?

    Regards,
    Somnath
  • Hi Somnath,

    I tried with the following changes:

    1)

    void dram_init_banksize(void)

    {

           u64 ram_size;

           ram_size = board_ti_get_emif_size();

           gd->bd->bi_dram[0].start = 0x200000000;           /*     Changed from CONFIG_SYS_SDRAM_BASE to 0x200000000* /;

           gd->bd->bi_dram[0].size = 0x80000000;                                                /*Changed from get_effective_memsize() to 0x80000000;*/

           if (ram_size > CONFIG_MAX_MEM_MAPPED) {

                   gd->bd->bi_dram[1].start = 0x200000000;

                   gd->bd->bi_dram[1].size = ram_size - CONFIG_MAX_MEM_MAPPED;

           }

    2)

    static const struct dmm_lisa_map_regs lisa_map_dra7_4GB = {
    .dmm_lisa_map_0 = 0x0,
    .dmm_lisa_map_1 = 0x80600100,
    .dmm_lisa_map_2 = 0xC0600200,
    .dmm_lisa_map_3 = 0xFF020100,
    .is_ma_present = 0x1
    };

    From the uboot it is still reading  2GB and it is getting stuck after that:

    Check the below logs:

    reading u-boot.img

    reading u-boot.img

    reading u-boot.img

    reading u-boot.img

    U-Boot 2016.05-00009-gac1d50f-dirty (Aug 06 2018 - 16:13:24 +0530)

    CPU  : DRA762-GP ES1.0

    Model: TI DRA762 EVM

    Board: DRA74x EVM REV

    DRAM:  2 GiB

    Thanks

    Deep

  • Hi Deep,

    Please leave  gd->bd->bi_dram[0].start and  gd->bd->bi_dram[0].size as the default.

    You should only need to change the following (and ensure that they are being set...if needed please comment out the "if" statement):

    gd->bd->bi_dram[1].start = 0x200000000;
    gd->bd->bi_dram[1].size = 0x80000000;

    Best regards,
    Kevin

  • Hi Kevin,

    Thanks for your reply.
    I tried with the changes above, the board booted this time, but the DRAM size identified by u-boot remained the same 2GB.
    Do we need to do any changes in device tree file of uboot also?

    Regards,
    Deep
  • Hi Deep,

    As far as I am aware, you shouldn't need to change any device tree file.

    Can you print out the value of ramsize and confirm that the bootloader code is entering the "if" statement (ramsize > CONFIG_MAX_MEM_MAPPED)?

    Best regards,
    Kevin
  • Hi Kevin,

    I will let you know the results by tommorow.

    Thanks
  • Hi Kevin,

    You were right,it was not going inside the  

    if (ram_size > CONFIG_MAX_MEM_MAPPED) 

    I tried to print the ram_size before if statement. It was coming zero.

    void dram_init_banksize(void)
    {
    u64 ram_size;
    ram_size = board_ti_get_emif_size();
    printf("**************Ramsize before if is %llu\n",ram_size);........................................Here it's coming zero

    gd->bd->bi_dram[0].start =CONFIG_SYS_SDRAM_BASE;
    gd->bd->bi_dram[0].size = get_effective_memsize();
    if (ram_size > CONFIG_MAX_MEM_MAPPED) {
    printf("**************Ramsize is %llu\n",ram_size); --------------------------------------------Not going inside if
    gd->bd->bi_dram[1].start = 0x200000000;
    gd->bd->bi_dram[1].size = 0x80000000;
    }
    }

    Should I try commenting if ??

    Regards

    Deep

  • Hi Deep,

    You could comment out the if statement or hard code ram_size to 4GB (shown below).

    //ram_size = board_ti_get_emif_size();
    ram_size = 0x100000000;

    Let us know if this doesn't fix the issue.

    Best regards,
    Kevin

  • Hi Kevin,

    Thanks for your reply.

    This is showing 4GB in uboot as shown below:


    U-Boot 2016.05-00009-gac1d50f-dirty (Aug 07 2018 - 19:38:04 +0530)

    CPU : DRA762-GP ES1.0
    Model: TI DRA762 EVM
    Board: DRA74x EVM REV
    DRAM: **************Ramsize before if is 4294967296
    **************Ramsize is 4294967296
    4 GiB

    But Is the uboot actually getting 4GB?
    Is there any tool to check the same in uboot?
    Also what changes should be done in device tree file for kernel?

    Thanks
    Deep


  • Hi Deep,

    The extended 2GB won't be accessible until LPAE is enabled. The kernel should enable LPAE.

    There should be nothing that is needed to change in the device tree file for the kernel; u-boot should pass the required information to the kernel.

    You can check the total memory from the kernel by typing >> cat /proc/meminfo

    Best regards,
    Kevin
  • Hi Kevin,

    Thanks for your reply. i will check the meminfo and let you know.
    Thanks a lot for your help.

    Regards
    Deep
  • Hi Kevin,

    I checked the kernel logs by:

    cat /proc/meminfo

    root@dra7xx-evm:~# cat /proc/meminfo 
    MemTotal:         533064 kB            ---------520MB
    MemFree:          336828 kB
    MemAvailable:     447376 kB
    Buffers:            7724 kB
    Cached:            96680 kB
    SwapCached:            0 kB
    Active:            43536 kB
    Inactive:          73212 kB
    Active(anon):      13708 kB
    Inactive(anon):     3500 kB
    Active(file):      29828 kB
    Inactive(file):    69712 kB
    Unevictable:           0 kB
    Mlocked:               0 kB
    HighTotal:        258048 kB
    HighFree:         170128 kB
    LowTotal:         275016 kB
    LowFree:          166700 kB
    SwapTotal:             0 kB
    SwapFree:              0 kB
    Dirty:              1832 kB
    Writeback:             0 kB
    AnonPages:         12344 kB
    Mapped:            15204 kB
    Shmem:              4860 kB
    Slab:              29596 kB
    SReclaimable:      18940 kB
    SUnreclaim:        10656 kB
    KernelStack:         968 kB
    PageTables:          588 kB
    NFS_Unstable:          0 kB
    Bounce:                0 kB
    WritebackTmp:          0 kB
    CommitLimit:      266532 kB
    Committed_AS:     171000 kB
    VmallocTotal:     245760 kB
    VmallocUsed:           0 kB
    VmallocChunk:          0 kB
    CmaTotal:         204800 kB
    CmaFree:          161908 kB

    I have compiled  using 

    MAKECONFIG=tda2px_evm_linux_all   in Vision SDK  PROCESSOR_SDK_VISION_03_03_00_00

    I think we need to change in the  mem_segment_definition_linux.xs the size of DDR3.

    Do you have any suggestions on this?

    Thanks

    Deep

  • Hi Deep,

    Vision SDK doesn't support 4GB.

    Regards,
    Stanley
  • Hi Stanley
    Thanks for your reply.
    So VSDK Linux will also not support 4GB.
    Upto which memory can VSDK support?
    Thanks
    Deep
  • Hi,

    Can anyone please reply on this?

    Thanks

    Deep

  • Former Member
    0 Former Member in reply to deepikateriar
    Hi,
    It can support upto 2GB.

    Regards,
    Somnath
  • Thanks Somnath,

    Will come back to you in case of any further query.
    Regards,
    Deep