This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2PXEVM: The size limitation of issm2misp scaler?

Part Number: TDA2PXEVM

Tool/software: Linux

Hi All,

There's a problem in issm2misp scaler.
If the input resolution is 2880x1080 and output is 1920x1080, the output image is broken at left 64 and rift 64pixels of output width 1920. And if the input size is reduced to 2816x1080, it's ok.

What's the limitation of issm2misp scaler? Max. size or multiple of 128 (2816 is multiple of 128 but 2880 is of 64)??

Thanks.