This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138B-EP: OMAPL138 - VPIF

Part Number: OMAPL138B-EP
Other Parts Discussed in Thread: OMAPL138

Hello,

I recently asked questions about VPIF.
The following link is a question that I posted a while ago.

e2e.ti.com/.../743474


I've read answers and some have helped, but I still have some questions.

The OMAPL138 Technical Reference Manual states that VPIF supports BT.656, BT.1120, and SMTPE 296. I am trying to receive data in SMTPE 296 format (1280x720p).
The description of the Technical Reference Manual is based on SMTPE 296 (progressive, 60 fps). Now I am trying to receive data with SMTPE 296 (progressive, 30 fps).
However, the VPIF interrupt does not working and no data is received from the camera.

The register settings are as follows.

C0CTRL - FIELDFRAME : 1
- INTRPROG : 1
- INTFRAME : 0
- YCMUX : 0
- CAPMODE : 0
- CHANEN : 1

C1CTRL - INTRPROG : 1
- YCMUX : 0
- CAPMODE : 0
- CHANEN : 1

INTEN - ERROR : 1
- FRAME0 : 1
INTSET - ERROR : 1
- FRAME0 : 1

ch0, ch1 is same(Only CnHCFG(EAV2SAV) is different from the number shown in Technical Reference Manual)
CnTLUMA - n is 0 : Luma Buffer Addr, 1 : Chroma Buffer Addr.
CnHCFG - EAV2SAV : 2012(30fps) / manual is 362 (it seems to be based on 60fps)
- SAV2EAV : 1280
CnVCFG0 - L1 : 1
- L3 : 26
CnVCFG1 - L5 : 746
CnVSIZE - VSIZE : 750

The other register setting is 0.

Among the answers (second link), BT.1120 (FHD, 1920x1080, 30p) is not supported by OMAPL138.
However, the Technical Reference Manual clearly states that it is supported.
I'm wondering if SMTPE 296 (HD, 1280x720) is not supported either.
If it is not, please give me a guide.

Thank you.

  • And there is one more question.

    My camera (SMTPE 296 format) is transmitting active data when the VSYNC and HSYNC signals are low.
    However, in 'Figure 36-5. Progressive Video' of the Technical Reference Manual of OMAPL138, active data is transmitted when VSYNC and HSYNC are high.

    I'm wondering if this difference is related to the SMTPE 296 format not receiving the data.
  • Hi,

    I will find out about the support for SMTPE 296 (progressive, 30 fps).
    In your other post, you said that no OS is being used. What software did you start with?

    Regards,
    Mark
  • Hi,

    I'm awaiting feedback on this still. I'm no VIP expert, but I noticed that in the datasheet Table 6-121. Timing Requirements for VPIF VP_CLKINx Inputs, the fastest supported clock frequency is 75.188MHz.

    You stated that your camera outputs 148.5MHz. Could this be the issue? And the reason why BT.1120 (FHD, 1920x1080, 30p) is also not supported? If so, I don't know why it was pusblished as such in the TRM...

    Does the camera support slower modes of operation with the same signaling polarity that we can use to debug this issue?

    Regards,
    Mark
  • Mark, thank you for your reply.
    And I am sorry that the feedback is slow. I have not been in the office for a few days.

    First of all, what I am currently doing is just taking the camera data and outputting it to the LCD (without OS)
    We have successfully implemented the BT.656 format using OMAPL138's VPIF and LCDC.

    And the next step is to receive the data from the camera in SMTPE 296 (progressive, 30 fps, 1280 * 720) format and print it out on the LCD.
    My current camera is output in SMTPE 296 (progressive, 30 fps, 1280 * 720, 74.25MHz) format.
    And I have not mentioned that my camera outputs 148.5MHz.

    And to say that the OMAPL138 does not support BT.1120 (FHD, 1920x1080, 30p), I saw the TI forum article (link below).
    e2e.ti.com/.../639095

    We would appreciate it if you also informed us that the register settings for receiving data in SMTPE 296 (progressive, 30 fps, 1280 * 720) format are correct.


    In addition, BT656 (720x240 / 288) (interlaced, 60 fields @ 27MHz) was successfully implemented,
    but I wonder if max. D1 (720x480) YCbCr422 / RGB565 / RGB444. (Progressive, 60 fps @ 54MHz) can receive data via VPIF.
    I also wonder if there is a max frame that OMAPL138 VPIF can handle (whether it is 60 fps or just 30 fps).

    Thank you.
  • Hi,

    Sorry for the delay on this thread. I will follow up with the VIP expert tomorrow.

    Regards,
    Mark
  • wonjune kim said:
    I also wonder if there is a max frame that OMAPL138 VPIF can handle (whether it is 60 fps or just 30 fps).

    If the particular resolution is supported by VPIF IP, then FPS support for that resolution depends upon the max pixel clock frequency supported by VPIF IP. If the pixel clock frequency needed to capture @ 60 fps is beyond what IP can support, you should lower fps capture, but  I wouldn't expect to see no capture. 

  • manisha, thank you for your reply.

    It helped me a lot.
    But the biggest question I have is whether I can receive data in SMTPE 296 (progressive, 30 fps, 1280 * 720) format via OMAPL138's VPIF.

    Can you answer that question?

    If there is a problem with the register value I set in relation to this problem, please give feedback.

    Thank you very much.
  • Hi,

    I assume you are using Processor SDK Linux software

    You may want to refer to linux driver  inside board-support/linux-xxxxxx/drivers/media/platform/davinci/vpif_capture.c for SPMTE capture settings.

    Please also check this e2e post

    Regards,

    Manisha

  • manisha, thank you for your reply.

    Unfortunately, I do not use Linux.(we are in the process without OS)

    And now it is difficult to build a Linux environment.
    If you can, can you upload the vpif_capture.c file mentioned in the answer?
    Otherwise, it would be appreciated if you let me know register settings about the SMTPE 296 (progressive, 60 fps) format.


    Thank you very much.
  • Please find attached linux file

    /*
     * Copyright (C) 2009 Texas Instruments Inc
     * Copyright (C) 2014 Lad, Prabhakar <prabhakar.csengg@gmail.com>
     *
     * This program is free software; you can redistribute it and/or modify
     * it under the terms of the GNU General Public License as published by
     * the Free Software Foundation; either version 2 of the License, or
     * (at your option) any later version.
     *
     * This program is distributed in the hope that it will be useful,
     * but WITHOUT ANY WARRANTY; without even the implied warranty of
     * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
     * GNU General Public License for more details.
     *
     * TODO : add support for VBI & HBI data service
     *	  add static buffer allocation
     */
    
    #include <linux/module.h>
    #include <linux/interrupt.h>
    #include <linux/of_graph.h>
    #include <linux/platform_device.h>
    #include <linux/slab.h>
    
    #include <media/v4l2-fwnode.h>
    #include <media/v4l2-ioctl.h>
    #include <media/i2c/tvp514x.h>
    #include <media/v4l2-mediabus.h>
    
    #include <linux/videodev2.h>
    
    #include "vpif.h"
    #include "vpif_capture.h"
    
    MODULE_DESCRIPTION("TI DaVinci VPIF Capture driver");
    MODULE_LICENSE("GPL");
    MODULE_VERSION(VPIF_CAPTURE_VERSION);
    
    #define vpif_err(fmt, arg...)	v4l2_err(&vpif_obj.v4l2_dev, fmt, ## arg)
    #define vpif_dbg(level, debug, fmt, arg...)	\
    		v4l2_dbg(level, debug, &vpif_obj.v4l2_dev, fmt, ## arg)
    
    static int debug = 1;
    
    module_param(debug, int, 0644);
    
    MODULE_PARM_DESC(debug, "Debug level 0-1");
    
    #define VPIF_DRIVER_NAME	"vpif_capture"
    MODULE_ALIAS("platform:" VPIF_DRIVER_NAME);
    
    /* global variables */
    static struct vpif_device vpif_obj = { {NULL} };
    static struct device *vpif_dev;
    static void vpif_calculate_offsets(struct channel_obj *ch);
    static void vpif_config_addr(struct channel_obj *ch, int muxmode);
    
    static u8 channel_first_int[VPIF_NUMBER_OF_OBJECTS][2] = { {1, 1} };
    
    /* Is set to 1 in case of SDTV formats, 2 in case of HDTV formats. */
    static int ycmux_mode;
    
    static inline
    struct vpif_cap_buffer *to_vpif_buffer(struct vb2_v4l2_buffer *vb)
    {
    	return container_of(vb, struct vpif_cap_buffer, vb);
    }
    
    /**
     * vpif_buffer_prepare :  callback function for buffer prepare
     * @vb: ptr to vb2_buffer
     *
     * This is the callback function for buffer prepare when vb2_qbuf()
     * function is called. The buffer is prepared and user space virtual address
     * or user address is converted into  physical address
     */
    static int vpif_buffer_prepare(struct vb2_buffer *vb)
    {
    	struct vb2_v4l2_buffer *vbuf = to_vb2_v4l2_buffer(vb);
    	struct vb2_queue *q = vb->vb2_queue;
    	struct channel_obj *ch = vb2_get_drv_priv(q);
    	struct common_obj *common;
    	unsigned long addr;
    
    	vpif_dbg(2, debug, "vpif_buffer_prepare\n");
    
    	common = &ch->common[VPIF_VIDEO_INDEX];
    
    	vb2_set_plane_payload(vb, 0, common->fmt.fmt.pix.sizeimage);
    	if (vb2_get_plane_payload(vb, 0) > vb2_plane_size(vb, 0))
    		return -EINVAL;
    
    	vbuf->field = common->fmt.fmt.pix.field;
    
    	addr = vb2_dma_contig_plane_dma_addr(vb, 0);
    	if (!IS_ALIGNED((addr + common->ytop_off), 8) ||
    		!IS_ALIGNED((addr + common->ybtm_off), 8) ||
    		!IS_ALIGNED((addr + common->ctop_off), 8) ||
    		!IS_ALIGNED((addr + common->cbtm_off), 8)) {
    		vpif_dbg(1, debug, "offset is not aligned\n");
    		return -EINVAL;
    	}
    
    	return 0;
    }
    
    /**
     * vpif_buffer_queue_setup : Callback function for buffer setup.
     * @vq: vb2_queue ptr
     * @nbuffers: ptr to number of buffers requested by application
     * @nplanes:: contains number of distinct video planes needed to hold a frame
     * @sizes[]: contains the size (in bytes) of each plane.
     * @alloc_devs: ptr to allocation context
     *
     * This callback function is called when reqbuf() is called to adjust
     * the buffer count and buffer size
     */
    static int vpif_buffer_queue_setup(struct vb2_queue *vq,
    				unsigned int *nbuffers, unsigned int *nplanes,
    				unsigned int sizes[], struct device *alloc_devs[])
    {
    	struct channel_obj *ch = vb2_get_drv_priv(vq);
    	struct common_obj *common = &ch->common[VPIF_VIDEO_INDEX];
    	unsigned size = common->fmt.fmt.pix.sizeimage;
    
    	vpif_dbg(2, debug, "vpif_buffer_setup\n");
    
    	if (*nplanes) {
    		if (sizes[0] < size)
    			return -EINVAL;
    		size = sizes[0];
    	}
    
    	if (vq->num_buffers + *nbuffers < 3)
    		*nbuffers = 3 - vq->num_buffers;
    
    	*nplanes = 1;
    	sizes[0] = size;
    
    	/* Calculate the offset for Y and C data in the buffer */
    	vpif_calculate_offsets(ch);
    
    	return 0;
    }
    
    /**
     * vpif_buffer_queue : Callback function to add buffer to DMA queue
     * @vb: ptr to vb2_buffer
     */
    static void vpif_buffer_queue(struct vb2_buffer *vb)
    {
    	struct vb2_v4l2_buffer *vbuf = to_vb2_v4l2_buffer(vb);
    	struct channel_obj *ch = vb2_get_drv_priv(vb->vb2_queue);
    	struct vpif_cap_buffer *buf = to_vpif_buffer(vbuf);
    	struct common_obj *common;
    	unsigned long flags;
    
    	common = &ch->common[VPIF_VIDEO_INDEX];
    
    	vpif_dbg(2, debug, "vpif_buffer_queue\n");
    
    	spin_lock_irqsave(&common->irqlock, flags);
    	/* add the buffer to the DMA queue */
    	list_add_tail(&buf->list, &common->dma_queue);
    	spin_unlock_irqrestore(&common->irqlock, flags);
    }
    
    /**
     * vpif_start_streaming : Starts the DMA engine for streaming
     * @vb: ptr to vb2_buffer
     * @count: number of buffers
     */
    static int vpif_start_streaming(struct vb2_queue *vq, unsigned int count)
    {
    	struct vpif_capture_config *vpif_config_data =
    					vpif_dev->platform_data;
    	struct channel_obj *ch = vb2_get_drv_priv(vq);
    	struct common_obj *common = &ch->common[VPIF_VIDEO_INDEX];
    	struct vpif_params *vpif = &ch->vpifparams;
    	struct vpif_cap_buffer *buf, *tmp;
    	unsigned long addr, flags;
    	int ret;
    
    	/* Initialize field_id */
    	ch->field_id = 0;
    
    	/* configure 1 or 2 channel mode */
    	if (vpif_config_data->setup_input_channel_mode) {
    		ret = vpif_config_data->
    			setup_input_channel_mode(vpif->std_info.ycmux_mode);
    		if (ret < 0) {
    			vpif_dbg(1, debug, "can't set vpif channel mode\n");
    			goto err;
    		}
    	}
    
    	ret = v4l2_subdev_call(ch->sd, video, s_stream, 1);
    	if (ret && ret != -ENOIOCTLCMD && ret != -ENODEV) {
    		vpif_dbg(1, debug, "stream on failed in subdev\n");
    		goto err;
    	}
    
    	/* Call vpif_set_params function to set the parameters and addresses */
    	ret = vpif_set_video_params(vpif, ch->channel_id);
    	if (ret < 0) {
    		vpif_dbg(1, debug, "can't set video params\n");
    		goto err;
    	}
    
    	ycmux_mode = ret;
    	vpif_config_addr(ch, ret);
    
    	/* Get the next frame from the buffer queue */
    	spin_lock_irqsave(&common->irqlock, flags);
    	common->cur_frm = common->next_frm = list_entry(common->dma_queue.next,
    				    struct vpif_cap_buffer, list);
    	/* Remove buffer from the buffer queue */
    	list_del(&common->cur_frm->list);
    	spin_unlock_irqrestore(&common->irqlock, flags);
    
    	addr = vb2_dma_contig_plane_dma_addr(&common->cur_frm->vb.vb2_buf, 0);
    
    	common->set_addr(addr + common->ytop_off,
    			 addr + common->ybtm_off,
    			 addr + common->ctop_off,
    			 addr + common->cbtm_off);
    
    	/**
    	 * Set interrupt for both the fields in VPIF Register enable channel in
    	 * VPIF register
    	 */
    	channel_first_int[VPIF_VIDEO_INDEX][ch->channel_id] = 1;
    	if (VPIF_CHANNEL0_VIDEO == ch->channel_id) {
    		channel0_intr_assert();
    		channel0_intr_enable(1);
    		enable_channel0(1);
    	}
    	if (VPIF_CHANNEL1_VIDEO == ch->channel_id ||
    		ycmux_mode == 2) {
    		channel1_intr_assert();
    		channel1_intr_enable(1);
    		enable_channel1(1);
    	}
    
    	return 0;
    
    err:
    	spin_lock_irqsave(&common->irqlock, flags);
    	list_for_each_entry_safe(buf, tmp, &common->dma_queue, list) {
    		list_del(&buf->list);
    		vb2_buffer_done(&buf->vb.vb2_buf, VB2_BUF_STATE_QUEUED);
    	}
    	spin_unlock_irqrestore(&common->irqlock, flags);
    
    	return ret;
    }
    
    /**
     * vpif_stop_streaming : Stop the DMA engine
     * @vq: ptr to vb2_queue
     *
     * This callback stops the DMA engine and any remaining buffers
     * in the DMA queue are released.
     */
    static void vpif_stop_streaming(struct vb2_queue *vq)
    {
    	struct channel_obj *ch = vb2_get_drv_priv(vq);
    	struct common_obj *common;
    	unsigned long flags;
    	int ret;
    
    	common = &ch->common[VPIF_VIDEO_INDEX];
    
    	/* Disable channel as per its device type and channel id */
    	if (VPIF_CHANNEL0_VIDEO == ch->channel_id) {
    		enable_channel0(0);
    		channel0_intr_enable(0);
    	}
    	if (VPIF_CHANNEL1_VIDEO == ch->channel_id ||
    		ycmux_mode == 2) {
    		enable_channel1(0);
    		channel1_intr_enable(0);
    	}
    
    	ycmux_mode = 0;
    
    	ret = v4l2_subdev_call(ch->sd, video, s_stream, 0);
    	if (ret && ret != -ENOIOCTLCMD && ret != -ENODEV)
    		vpif_dbg(1, debug, "stream off failed in subdev\n");
    
    	/* release all active buffers */
    	if (common->cur_frm == common->next_frm) {
    		vb2_buffer_done(&common->cur_frm->vb.vb2_buf,
    				VB2_BUF_STATE_ERROR);
    	} else {
    		if (common->cur_frm)
    			vb2_buffer_done(&common->cur_frm->vb.vb2_buf,
    					VB2_BUF_STATE_ERROR);
    		if (common->next_frm)
    			vb2_buffer_done(&common->next_frm->vb.vb2_buf,
    					VB2_BUF_STATE_ERROR);
    	}
    
    	spin_lock_irqsave(&common->irqlock, flags);
    	while (!list_empty(&common->dma_queue)) {
    		common->next_frm = list_entry(common->dma_queue.next,
    						struct vpif_cap_buffer, list);
    		list_del(&common->next_frm->list);
    		vb2_buffer_done(&common->next_frm->vb.vb2_buf,
    				VB2_BUF_STATE_ERROR);
    	}
    	spin_unlock_irqrestore(&common->irqlock, flags);
    }
    
    static const struct vb2_ops video_qops = {
    	.queue_setup		= vpif_buffer_queue_setup,
    	.buf_prepare		= vpif_buffer_prepare,
    	.start_streaming	= vpif_start_streaming,
    	.stop_streaming		= vpif_stop_streaming,
    	.buf_queue		= vpif_buffer_queue,
    	.wait_prepare		= vb2_ops_wait_prepare,
    	.wait_finish		= vb2_ops_wait_finish,
    };
    
    /**
     * vpif_process_buffer_complete: process a completed buffer
     * @common: ptr to common channel object
     *
     * This function time stamp the buffer and mark it as DONE. It also
     * wake up any process waiting on the QUEUE and set the next buffer
     * as current
     */
    static void vpif_process_buffer_complete(struct common_obj *common)
    {
    	common->cur_frm->vb.vb2_buf.timestamp = ktime_get_ns();
    	vb2_buffer_done(&common->cur_frm->vb.vb2_buf, VB2_BUF_STATE_DONE);
    	/* Make curFrm pointing to nextFrm */
    	common->cur_frm = common->next_frm;
    }
    
    /**
     * vpif_schedule_next_buffer: set next buffer address for capture
     * @common : ptr to common channel object
     *
     * This function will get next buffer from the dma queue and
     * set the buffer address in the vpif register for capture.
     * the buffer is marked active
     */
    static void vpif_schedule_next_buffer(struct common_obj *common)
    {
    	unsigned long addr = 0;
    
    	spin_lock(&common->irqlock);
    	common->next_frm = list_entry(common->dma_queue.next,
    				     struct vpif_cap_buffer, list);
    	/* Remove that buffer from the buffer queue */
    	list_del(&common->next_frm->list);
    	spin_unlock(&common->irqlock);
    	addr = vb2_dma_contig_plane_dma_addr(&common->next_frm->vb.vb2_buf, 0);
    
    	/* Set top and bottom field addresses in VPIF registers */
    	common->set_addr(addr + common->ytop_off,
    			 addr + common->ybtm_off,
    			 addr + common->ctop_off,
    			 addr + common->cbtm_off);
    }
    
    /**
     * vpif_channel_isr : ISR handler for vpif capture
     * @irq: irq number
     * @dev_id: dev_id ptr
     *
     * It changes status of the captured buffer, takes next buffer from the queue
     * and sets its address in VPIF registers
     */
    static irqreturn_t vpif_channel_isr(int irq, void *dev_id)
    {
    	struct vpif_device *dev = &vpif_obj;
    	struct common_obj *common;
    	struct channel_obj *ch;
    	int channel_id;
    	int fid = -1, i;
    
    	channel_id = *(int *)(dev_id);
    	if (!vpif_intr_status(channel_id))
    		return IRQ_NONE;
    
    	ch = dev->dev[channel_id];
    
    	for (i = 0; i < VPIF_NUMBER_OF_OBJECTS; i++) {
    		common = &ch->common[i];
    		/* skip If streaming is not started in this channel */
    		/* Check the field format */
    		if (1 == ch->vpifparams.std_info.frm_fmt ||
    		    common->fmt.fmt.pix.field == V4L2_FIELD_NONE) {
    			/* Progressive mode */
    			spin_lock(&common->irqlock);
    			if (list_empty(&common->dma_queue)) {
    				spin_unlock(&common->irqlock);
    				continue;
    			}
    			spin_unlock(&common->irqlock);
    
    			if (!channel_first_int[i][channel_id])
    				vpif_process_buffer_complete(common);
    
    			channel_first_int[i][channel_id] = 0;
    
    			vpif_schedule_next_buffer(common);
    
    
    			channel_first_int[i][channel_id] = 0;
    		} else {
    			/**
    			 * Interlaced mode. If it is first interrupt, ignore
    			 * it
    			 */
    			if (channel_first_int[i][channel_id]) {
    				channel_first_int[i][channel_id] = 0;
    				continue;
    			}
    			if (0 == i) {
    				ch->field_id ^= 1;
    				/* Get field id from VPIF registers */
    				fid = vpif_channel_getfid(ch->channel_id);
    				if (fid != ch->field_id) {
    					/**
    					 * If field id does not match stored
    					 * field id, make them in sync
    					 */
    					if (0 == fid)
    						ch->field_id = fid;
    					return IRQ_HANDLED;
    				}
    			}
    			/* device field id and local field id are in sync */
    			if (0 == fid) {
    				/* this is even field */
    				if (common->cur_frm == common->next_frm)
    					continue;
    
    				/* mark the current buffer as done */
    				vpif_process_buffer_complete(common);
    			} else if (1 == fid) {
    				/* odd field */
    				spin_lock(&common->irqlock);
    				if (list_empty(&common->dma_queue) ||
    				    (common->cur_frm != common->next_frm)) {
    					spin_unlock(&common->irqlock);
    					continue;
    				}
    				spin_unlock(&common->irqlock);
    
    				vpif_schedule_next_buffer(common);
    			}
    		}
    	}
    	return IRQ_HANDLED;
    }
    
    /**
     * vpif_update_std_info() - update standard related info
     * @ch: ptr to channel object
     *
     * For a given standard selected by application, update values
     * in the device data structures
     */
    static int vpif_update_std_info(struct channel_obj *ch)
    {
    	struct common_obj *common = &ch->common[VPIF_VIDEO_INDEX];
    	struct vpif_params *vpifparams = &ch->vpifparams;
    	const struct vpif_channel_config_params *config;
    	struct vpif_channel_config_params *std_info = &vpifparams->std_info;
    	struct video_obj *vid_ch = &ch->video;
    	int index;
    	struct v4l2_pix_format *pixfmt = &common->fmt.fmt.pix;
    
    	vpif_dbg(2, debug, "vpif_update_std_info\n");
    
    	/*
    	 * if called after try_fmt or g_fmt, there will already be a size
    	 * so use that by default.
    	 */
    	if (pixfmt->width && pixfmt->height) {
    		if (pixfmt->field == V4L2_FIELD_ANY ||
    		    pixfmt->field == V4L2_FIELD_NONE)
    			pixfmt->field = V4L2_FIELD_NONE;
    
    		vpifparams->iface.if_type = VPIF_IF_BT656;
    		if (pixfmt->pixelformat == V4L2_PIX_FMT_SGRBG10 ||
    		    pixfmt->pixelformat == V4L2_PIX_FMT_SBGGR8)
    			vpifparams->iface.if_type = VPIF_IF_RAW_BAYER;
    
    		if (pixfmt->pixelformat == V4L2_PIX_FMT_SGRBG10)
    			vpifparams->params.data_sz = 1; /* 10 bits/pixel.  */
    
    		/*
    		 * For raw formats from camera sensors, we don't need
    		 * the std_info from table lookup, so nothing else to do here.
    		 */
    		if (vpifparams->iface.if_type == VPIF_IF_RAW_BAYER) {
    			memset(std_info, 0, sizeof(struct vpif_channel_config_params));
    			vpifparams->std_info.capture_format = 1; /* CCD/raw mode */
    			return 0;
    		}
    	}
    
    	for (index = 0; index < vpif_ch_params_count; index++) {
    		config = &vpif_ch_params[index];
    		if (config->hd_sd == 0) {
    			vpif_dbg(2, debug, "SD format\n");
    			if (config->stdid & vid_ch->stdid) {
    				memcpy(std_info, config, sizeof(*config));
    				break;
    			}
    		} else {
    			vpif_dbg(2, debug, "HD format\n");
    			if (!memcmp(&config->dv_timings, &vid_ch->dv_timings,
    				sizeof(vid_ch->dv_timings))) {
    				memcpy(std_info, config, sizeof(*config));
    				break;
    			}
    		}
    	}
    
    	/* standard not found */
    	if (index == vpif_ch_params_count)
    		return -EINVAL;
    
    	common->fmt.fmt.pix.width = std_info->width;
    	common->width = std_info->width;
    	common->fmt.fmt.pix.height = std_info->height;
    	common->height = std_info->height;
    	common->fmt.fmt.pix.sizeimage = common->height * common->width * 2;
    	common->fmt.fmt.pix.bytesperline = std_info->width;
    	vpifparams->video_params.hpitch = std_info->width;
    	vpifparams->video_params.storage_mode = std_info->frm_fmt;
    
    	if (vid_ch->stdid)
    		common->fmt.fmt.pix.colorspace = V4L2_COLORSPACE_SMPTE170M;
    	else
    		common->fmt.fmt.pix.colorspace = V4L2_COLORSPACE_REC709;
    
    	if (ch->vpifparams.std_info.frm_fmt)
    		common->fmt.fmt.pix.field = V4L2_FIELD_NONE;
    	else
    		common->fmt.fmt.pix.field = V4L2_FIELD_INTERLACED;
    
    	if (ch->vpifparams.iface.if_type == VPIF_IF_RAW_BAYER)
    		common->fmt.fmt.pix.pixelformat = V4L2_PIX_FMT_SBGGR8;
    	else
    		common->fmt.fmt.pix.pixelformat = V4L2_PIX_FMT_NV16;
    
    	common->fmt.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
    
    	return 0;
    }
    
    /**
     * vpif_calculate_offsets : This function calculates buffers offsets
     * @ch : ptr to channel object
     *
     * This function calculates buffer offsets for Y and C in the top and
     * bottom field
     */
    static void vpif_calculate_offsets(struct channel_obj *ch)
    {
    	unsigned int hpitch, sizeimage;
    	struct video_obj *vid_ch = &(ch->video);
    	struct vpif_params *vpifparams = &ch->vpifparams;
    	struct common_obj *common = &ch->common[VPIF_VIDEO_INDEX];
    	enum v4l2_field field = common->fmt.fmt.pix.field;
    
    	vpif_dbg(2, debug, "vpif_calculate_offsets\n");
    
    	if (V4L2_FIELD_ANY == field) {
    		if (vpifparams->std_info.frm_fmt)
    			vid_ch->buf_field = V4L2_FIELD_NONE;
    		else
    			vid_ch->buf_field = V4L2_FIELD_INTERLACED;
    	} else
    		vid_ch->buf_field = common->fmt.fmt.pix.field;
    
    	sizeimage = common->fmt.fmt.pix.sizeimage;
    
    	hpitch = common->fmt.fmt.pix.bytesperline;
    
    	if ((V4L2_FIELD_NONE == vid_ch->buf_field) ||
    	    (V4L2_FIELD_INTERLACED == vid_ch->buf_field)) {
    		/* Calculate offsets for Y top, Y Bottom, C top and C Bottom */
    		common->ytop_off = 0;
    		common->ybtm_off = hpitch;
    		common->ctop_off = sizeimage / 2;
    		common->cbtm_off = sizeimage / 2 + hpitch;
    	} else if (V4L2_FIELD_SEQ_TB == vid_ch->buf_field) {
    		/* Calculate offsets for Y top, Y Bottom, C top and C Bottom */
    		common->ytop_off = 0;
    		common->ybtm_off = sizeimage / 4;
    		common->ctop_off = sizeimage / 2;
    		common->cbtm_off = common->ctop_off + sizeimage / 4;
    	} else if (V4L2_FIELD_SEQ_BT == vid_ch->buf_field) {
    		/* Calculate offsets for Y top, Y Bottom, C top and C Bottom */
    		common->ybtm_off = 0;
    		common->ytop_off = sizeimage / 4;
    		common->cbtm_off = sizeimage / 2;
    		common->ctop_off = common->cbtm_off + sizeimage / 4;
    	}
    	if ((V4L2_FIELD_NONE == vid_ch->buf_field) ||
    	    (V4L2_FIELD_INTERLACED == vid_ch->buf_field))
    		vpifparams->video_params.storage_mode = 1;
    	else
    		vpifparams->video_params.storage_mode = 0;
    
    	if (1 == vpifparams->std_info.frm_fmt)
    		vpifparams->video_params.hpitch =
    		    common->fmt.fmt.pix.bytesperline;
    	else {
    		if ((field == V4L2_FIELD_ANY)
    		    || (field == V4L2_FIELD_INTERLACED))
    			vpifparams->video_params.hpitch =
    			    common->fmt.fmt.pix.bytesperline * 2;
    		else
    			vpifparams->video_params.hpitch =
    			    common->fmt.fmt.pix.bytesperline;
    	}
    
    	ch->vpifparams.video_params.stdid = vpifparams->std_info.stdid;
    }
    
    /**
     * vpif_get_default_field() - Get default field type based on interface
     * @vpif_params - ptr to vpif params
     */
    static inline enum v4l2_field vpif_get_default_field(
    				struct vpif_interface *iface)
    {
    	return (iface->if_type == VPIF_IF_RAW_BAYER) ? V4L2_FIELD_NONE :
    						V4L2_FIELD_INTERLACED;
    }
    
    /**
     * vpif_config_addr() - function to configure buffer address in vpif
     * @ch - channel ptr
     * @muxmode - channel mux mode
     */
    static void vpif_config_addr(struct channel_obj *ch, int muxmode)
    {
    	struct common_obj *common;
    
    	vpif_dbg(2, debug, "vpif_config_addr\n");
    
    	common = &(ch->common[VPIF_VIDEO_INDEX]);
    
    	if (VPIF_CHANNEL1_VIDEO == ch->channel_id)
    		common->set_addr = ch1_set_videobuf_addr;
    	else if (2 == muxmode)
    		common->set_addr = ch0_set_videobuf_addr_yc_nmux;
    	else
    		common->set_addr = ch0_set_videobuf_addr;
    }
    
    /**
     * vpif_input_to_subdev() - Maps input to sub device
     * @vpif_cfg - global config ptr
     * @chan_cfg - channel config ptr
     * @input_index - Given input index from application
     *
     * lookup the sub device information for a given input index.
     * we report all the inputs to application. inputs table also
     * has sub device name for the each input
     */
    static int vpif_input_to_subdev(
    		struct vpif_capture_config *vpif_cfg,
    		struct vpif_capture_chan_config *chan_cfg,
    		int input_index)
    {
    	struct vpif_subdev_info *subdev_info;
    	const char *subdev_name;
    	int i;
    
    	vpif_dbg(2, debug, "vpif_input_to_subdev\n");
    
    	if (!chan_cfg)
    		return -1;
    	if (input_index >= chan_cfg->input_count)
    		return -1;
    	subdev_name = chan_cfg->inputs[input_index].subdev_name;
    	if (!subdev_name)
    		return -1;
    
    	/* loop through the sub device list to get the sub device info */
    	for (i = 0; i < vpif_cfg->subdev_count; i++) {
    		subdev_info = &vpif_cfg->subdev_info[i];
    		if (subdev_info && !strcmp(subdev_info->name, subdev_name))
    			return i;
    	}
    	return -1;
    }
    
    /**
     * vpif_set_input() - Select an input
     * @vpif_cfg - global config ptr
     * @ch - channel
     * @_index - Given input index from application
     *
     * Select the given input.
     */
    static int vpif_set_input(
    		struct vpif_capture_config *vpif_cfg,
    		struct channel_obj *ch,
    		int index)
    {
    	struct vpif_capture_chan_config *chan_cfg =
    			&vpif_cfg->chan_config[ch->channel_id];
    	struct vpif_subdev_info *subdev_info = NULL;
    	struct v4l2_subdev *sd = NULL;
    	u32 input = 0, output = 0;
    	int sd_index;
    	int ret;
    
    	sd_index = vpif_input_to_subdev(vpif_cfg, chan_cfg, index);
    	if (sd_index >= 0) {
    		sd = vpif_obj.sd[sd_index];
    		subdev_info = &vpif_cfg->subdev_info[sd_index];
    	} else {
    		/* no subdevice, no input to setup */
    		return 0;
    	}
    
    	/* first setup input path from sub device to vpif */
    	if (sd && vpif_cfg->setup_input_path) {
    		ret = vpif_cfg->setup_input_path(ch->channel_id,
    				       subdev_info->name);
    		if (ret < 0) {
    			vpif_dbg(1, debug, "couldn't setup input path for the" \
    			" sub device %s, for input index %d\n",
    			subdev_info->name, index);
    			return ret;
    		}
    	}
    
    	if (sd) {
    		input = chan_cfg->inputs[index].input_route;
    		output = chan_cfg->inputs[index].output_route;
    		ret = v4l2_subdev_call(sd, video, s_routing,
    				input, output, 0);
    		if (ret < 0 && ret != -ENOIOCTLCMD) {
    			vpif_dbg(1, debug, "Failed to set input\n");
    			return ret;
    		}
    	}
    	ch->input_idx = index;
    	ch->sd = sd;
    	/* copy interface parameters to vpif */
    	ch->vpifparams.iface = chan_cfg->vpif_if;
    
    	/* update tvnorms from the sub device input info */
    	ch->video_dev.tvnorms = chan_cfg->inputs[index].input.std;
    	return 0;
    }
    
    /**
     * vpif_querystd() - querystd handler
     * @file: file ptr
     * @priv: file handle
     * @std_id: ptr to std id
     *
     * This function is called to detect standard at the selected input
     */
    static int vpif_querystd(struct file *file, void *priv, v4l2_std_id *std_id)
    {
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    	int ret;
    
    	vpif_dbg(2, debug, "vpif_querystd\n");
    
    	/* Call querystd function of decoder device */
    	ret = v4l2_subdev_call(ch->sd, video, querystd, std_id);
    
    	if (ret == -ENOIOCTLCMD || ret == -ENODEV)
    		return -ENODATA;
    	if (ret) {
    		vpif_dbg(1, debug, "Failed to query standard for sub devices\n");
    		return ret;
    	}
    
    	return 0;
    }
    
    /**
     * vpif_g_std() - get STD handler
     * @file: file ptr
     * @priv: file handle
     * @std_id: ptr to std id
     */
    static int vpif_g_std(struct file *file, void *priv, v4l2_std_id *std)
    {
    	struct vpif_capture_config *config = vpif_dev->platform_data;
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    	struct vpif_capture_chan_config *chan_cfg;
    	struct v4l2_input input;
    
    	vpif_dbg(2, debug, "vpif_g_std\n");
    
    	if (!config->chan_config[ch->channel_id].inputs)
    		return -ENODATA;
    
    	chan_cfg = &config->chan_config[ch->channel_id];
    	input = chan_cfg->inputs[ch->input_idx].input;
    	if (input.capabilities != V4L2_IN_CAP_STD)
    		return -ENODATA;
    
    	*std = ch->video.stdid;
    	return 0;
    }
    
    /**
     * vpif_s_std() - set STD handler
     * @file: file ptr
     * @priv: file handle
     * @std_id: ptr to std id
     */
    static int vpif_s_std(struct file *file, void *priv, v4l2_std_id std_id)
    {
    	struct vpif_capture_config *config = vpif_dev->platform_data;
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    	struct common_obj *common = &ch->common[VPIF_VIDEO_INDEX];
    	struct vpif_capture_chan_config *chan_cfg;
    	struct v4l2_input input;
    	int ret;
    
    	vpif_dbg(2, debug, "vpif_s_std\n");
    
    	if (!config->chan_config[ch->channel_id].inputs)
    		return -ENODATA;
    
    	chan_cfg = &config->chan_config[ch->channel_id];
    	input = chan_cfg->inputs[ch->input_idx].input;
    	if (input.capabilities != V4L2_IN_CAP_STD)
    		return -ENODATA;
    
    	if (vb2_is_busy(&common->buffer_queue))
    		return -EBUSY;
    
    	/* Call encoder subdevice function to set the standard */
    	ch->video.stdid = std_id;
    	memset(&ch->video.dv_timings, 0, sizeof(ch->video.dv_timings));
    
    	/* Get the information about the standard */
    	if (vpif_update_std_info(ch)) {
    		vpif_err("Error getting the standard info\n");
    		return -EINVAL;
    	}
    
    	/* set standard in the sub device */
    	ret = v4l2_subdev_call(ch->sd, video, s_std, std_id);
    	if (ret && ret != -ENOIOCTLCMD && ret != -ENODEV) {
    		vpif_dbg(1, debug, "Failed to set standard for sub devices\n");
    		return ret;
    	}
    	return 0;
    }
    
    /**
     * vpif_enum_input() - ENUMINPUT handler
     * @file: file ptr
     * @priv: file handle
     * @input: ptr to input structure
     */
    static int vpif_enum_input(struct file *file, void *priv,
    				struct v4l2_input *input)
    {
    
    	struct vpif_capture_config *config = vpif_dev->platform_data;
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    	struct vpif_capture_chan_config *chan_cfg;
    
    	chan_cfg = &config->chan_config[ch->channel_id];
    
    	if (input->index >= chan_cfg->input_count)
    		return -EINVAL;
    
    	memcpy(input, &chan_cfg->inputs[input->index].input,
    		sizeof(*input));
    	return 0;
    }
    
    /**
     * vpif_g_input() - Get INPUT handler
     * @file: file ptr
     * @priv: file handle
     * @index: ptr to input index
     */
    static int vpif_g_input(struct file *file, void *priv, unsigned int *index)
    {
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    
    	*index = ch->input_idx;
    	return 0;
    }
    
    /**
     * vpif_s_input() - Set INPUT handler
     * @file: file ptr
     * @priv: file handle
     * @index: input index
     */
    static int vpif_s_input(struct file *file, void *priv, unsigned int index)
    {
    	struct vpif_capture_config *config = vpif_dev->platform_data;
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    	struct common_obj *common = &ch->common[VPIF_VIDEO_INDEX];
    	struct vpif_capture_chan_config *chan_cfg;
    
    	chan_cfg = &config->chan_config[ch->channel_id];
    
    	if (index >= chan_cfg->input_count)
    		return -EINVAL;
    
    	if (vb2_is_busy(&common->buffer_queue))
    		return -EBUSY;
    
    	return vpif_set_input(config, ch, index);
    }
    
    /**
     * vpif_enum_fmt_vid_cap() - ENUM_FMT handler
     * @file: file ptr
     * @priv: file handle
     * @index: input index
     */
    static int vpif_enum_fmt_vid_cap(struct file *file, void  *priv,
    					struct v4l2_fmtdesc *fmt)
    {
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    
    	if (fmt->index != 0) {
    		vpif_dbg(1, debug, "Invalid format index\n");
    		return -EINVAL;
    	}
    
    	/* Fill in the information about format */
    	if (ch->vpifparams.iface.if_type == VPIF_IF_RAW_BAYER) {
    		fmt->type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
    		strcpy(fmt->description, "Raw Mode -Bayer Pattern GrRBGb");
    		fmt->pixelformat = V4L2_PIX_FMT_SBGGR8;
    	} else {
    		fmt->type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
    		strcpy(fmt->description, "YCbCr4:2:2 Semi-Planar");
    		fmt->pixelformat = V4L2_PIX_FMT_NV16;
    	}
    	return 0;
    }
    
    /**
     * vpif_try_fmt_vid_cap() - TRY_FMT handler
     * @file: file ptr
     * @priv: file handle
     * @fmt: ptr to v4l2 format structure
     */
    static int vpif_try_fmt_vid_cap(struct file *file, void *priv,
    				struct v4l2_format *fmt)
    {
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    	struct v4l2_pix_format *pixfmt = &fmt->fmt.pix;
    	struct common_obj *common = &(ch->common[VPIF_VIDEO_INDEX]);
    
    	common->fmt = *fmt;
    	vpif_update_std_info(ch);
    
    	pixfmt->field = common->fmt.fmt.pix.field;
    	pixfmt->colorspace = common->fmt.fmt.pix.colorspace;
    	pixfmt->bytesperline = common->fmt.fmt.pix.width;
    	pixfmt->width = common->fmt.fmt.pix.width;
    	pixfmt->height = common->fmt.fmt.pix.height;
    	pixfmt->sizeimage = pixfmt->bytesperline * pixfmt->height * 2;
    	if (pixfmt->pixelformat == V4L2_PIX_FMT_SGRBG10) {
    		pixfmt->bytesperline = common->fmt.fmt.pix.width * 2;
    		pixfmt->sizeimage = pixfmt->bytesperline * pixfmt->height;
    	}
    	pixfmt->priv = 0;
    
    	dev_dbg(vpif_dev, "%s: %d x %d; pitch=%d pixelformat=0x%08x, field=%d, size=%d\n", __func__,
    		pixfmt->width, pixfmt->height,
    		pixfmt->bytesperline, pixfmt->pixelformat,
    		pixfmt->field, pixfmt->sizeimage);
    
    	return 0;
    }
    
    
    /**
     * vpif_g_fmt_vid_cap() - Set INPUT handler
     * @file: file ptr
     * @priv: file handle
     * @fmt: ptr to v4l2 format structure
     */
    static int vpif_g_fmt_vid_cap(struct file *file, void *priv,
    				struct v4l2_format *fmt)
    {
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    	struct common_obj *common = &ch->common[VPIF_VIDEO_INDEX];
    	struct v4l2_pix_format *pix_fmt = &fmt->fmt.pix;
    	struct v4l2_subdev_format format = {
    		.which = V4L2_SUBDEV_FORMAT_ACTIVE,
    	};
    	struct v4l2_mbus_framefmt *mbus_fmt = &format.format;
    	int ret;
    
    	/* Check the validity of the buffer type */
    	if (common->fmt.type != fmt->type)
    		return -EINVAL;
    
    	/* By default, use currently set fmt */
    	*fmt = common->fmt;
    
    	/* If subdev has get_fmt, use that to override */
    	ret = v4l2_subdev_call(ch->sd, pad, get_fmt, NULL, &format);
    	if (!ret && mbus_fmt->code) {
    		v4l2_fill_pix_format(pix_fmt, mbus_fmt);
    		pix_fmt->bytesperline = pix_fmt->width;
    		if (mbus_fmt->code == MEDIA_BUS_FMT_SGRBG10_1X10) {
    			/* e.g. mt9v032 */
    			pix_fmt->pixelformat = V4L2_PIX_FMT_SGRBG10;
    			pix_fmt->bytesperline = pix_fmt->width * 2;
    		} else if (mbus_fmt->code == MEDIA_BUS_FMT_UYVY8_2X8) {
    			/* e.g. tvp514x */
    			pix_fmt->pixelformat = V4L2_PIX_FMT_NV16;
    			pix_fmt->bytesperline = pix_fmt->width * 2;
    		} else {
    			dev_warn(vpif_dev, "%s: Unhandled media-bus format 0x%x\n",
    				 __func__, mbus_fmt->code);
    		}
    		pix_fmt->sizeimage = pix_fmt->bytesperline * pix_fmt->height;
    		dev_dbg(vpif_dev, "%s: %d x %d; pitch=%d, pixelformat=0x%08x, code=0x%x, field=%d, size=%d\n", __func__,
    			pix_fmt->width, pix_fmt->height,
    			pix_fmt->bytesperline, pix_fmt->pixelformat,
    			mbus_fmt->code, pix_fmt->field, pix_fmt->sizeimage);
    
    		common->fmt = *fmt;
    		vpif_update_std_info(ch);
    	}
    
    	return 0;
    }
    
    /**
     * vpif_s_fmt_vid_cap() - Set FMT handler
     * @file: file ptr
     * @priv: file handle
     * @fmt: ptr to v4l2 format structure
     */
    static int vpif_s_fmt_vid_cap(struct file *file, void *priv,
    				struct v4l2_format *fmt)
    {
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    	struct common_obj *common = &ch->common[VPIF_VIDEO_INDEX];
    	int ret;
    
    	vpif_dbg(2, debug, "%s\n", __func__);
    
    	if (vb2_is_busy(&common->buffer_queue))
    		return -EBUSY;
    
    	ret = vpif_try_fmt_vid_cap(file, priv, fmt);
    	if (ret)
    		return ret;
    
    	/* store the format in the channel object */
    	common->fmt = *fmt;
    	return 0;
    }
    
    /**
     * vpif_querycap() - QUERYCAP handler
     * @file: file ptr
     * @priv: file handle
     * @cap: ptr to v4l2_capability structure
     */
    static int vpif_querycap(struct file *file, void  *priv,
    				struct v4l2_capability *cap)
    {
    	struct vpif_capture_config *config = vpif_dev->platform_data;
    
    	cap->device_caps = V4L2_CAP_VIDEO_CAPTURE | V4L2_CAP_STREAMING;
    	cap->capabilities = cap->device_caps | V4L2_CAP_DEVICE_CAPS;
    	strlcpy(cap->driver, VPIF_DRIVER_NAME, sizeof(cap->driver));
    	snprintf(cap->bus_info, sizeof(cap->bus_info), "platform:%s",
    		 dev_name(vpif_dev));
    	strlcpy(cap->card, config->card_name, sizeof(cap->card));
    
    	return 0;
    }
    
    /**
     * vpif_enum_dv_timings() - ENUM_DV_TIMINGS handler
     * @file: file ptr
     * @priv: file handle
     * @timings: input timings
     */
    static int
    vpif_enum_dv_timings(struct file *file, void *priv,
    		     struct v4l2_enum_dv_timings *timings)
    {
    	struct vpif_capture_config *config = vpif_dev->platform_data;
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    	struct vpif_capture_chan_config *chan_cfg;
    	struct v4l2_input input;
    	int ret;
    
    	if (!config->chan_config[ch->channel_id].inputs)
    		return -ENODATA;
    
    	chan_cfg = &config->chan_config[ch->channel_id];
    	input = chan_cfg->inputs[ch->input_idx].input;
    	if (input.capabilities != V4L2_IN_CAP_DV_TIMINGS)
    		return -ENODATA;
    
    	timings->pad = 0;
    
    	ret = v4l2_subdev_call(ch->sd, pad, enum_dv_timings, timings);
    	if (ret == -ENOIOCTLCMD || ret == -ENODEV)
    		return -EINVAL;
    
    	return ret;
    }
    
    /**
     * vpif_query_dv_timings() - QUERY_DV_TIMINGS handler
     * @file: file ptr
     * @priv: file handle
     * @timings: input timings
     */
    static int
    vpif_query_dv_timings(struct file *file, void *priv,
    		      struct v4l2_dv_timings *timings)
    {
    	struct vpif_capture_config *config = vpif_dev->platform_data;
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    	struct vpif_capture_chan_config *chan_cfg;
    	struct v4l2_input input;
    	int ret;
    
    	if (!config->chan_config[ch->channel_id].inputs)
    		return -ENODATA;
    
    	chan_cfg = &config->chan_config[ch->channel_id];
    	input = chan_cfg->inputs[ch->input_idx].input;
    	if (input.capabilities != V4L2_IN_CAP_DV_TIMINGS)
    		return -ENODATA;
    
    	ret = v4l2_subdev_call(ch->sd, video, query_dv_timings, timings);
    	if (ret == -ENOIOCTLCMD || ret == -ENODEV)
    		return -ENODATA;
    
    	return ret;
    }
    
    /**
     * vpif_s_dv_timings() - S_DV_TIMINGS handler
     * @file: file ptr
     * @priv: file handle
     * @timings: digital video timings
     */
    static int vpif_s_dv_timings(struct file *file, void *priv,
    		struct v4l2_dv_timings *timings)
    {
    	struct vpif_capture_config *config = vpif_dev->platform_data;
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    	struct vpif_params *vpifparams = &ch->vpifparams;
    	struct vpif_channel_config_params *std_info = &vpifparams->std_info;
    	struct common_obj *common = &ch->common[VPIF_VIDEO_INDEX];
    	struct video_obj *vid_ch = &ch->video;
    	struct v4l2_bt_timings *bt = &vid_ch->dv_timings.bt;
    	struct vpif_capture_chan_config *chan_cfg;
    	struct v4l2_input input;
    	int ret;
    
    	if (!config->chan_config[ch->channel_id].inputs)
    		return -ENODATA;
    
    	chan_cfg = &config->chan_config[ch->channel_id];
    	input = chan_cfg->inputs[ch->input_idx].input;
    	if (input.capabilities != V4L2_IN_CAP_DV_TIMINGS)
    		return -ENODATA;
    
    	if (timings->type != V4L2_DV_BT_656_1120) {
    		vpif_dbg(2, debug, "Timing type not defined\n");
    		return -EINVAL;
    	}
    
    	if (vb2_is_busy(&common->buffer_queue))
    		return -EBUSY;
    
    	/* Configure subdevice timings, if any */
    	ret = v4l2_subdev_call(ch->sd, video, s_dv_timings, timings);
    	if (ret == -ENOIOCTLCMD || ret == -ENODEV)
    		ret = 0;
    	if (ret < 0) {
    		vpif_dbg(2, debug, "Error setting custom DV timings\n");
    		return ret;
    	}
    
    	if (!(timings->bt.width && timings->bt.height &&
    				(timings->bt.hbackporch ||
    				 timings->bt.hfrontporch ||
    				 timings->bt.hsync) &&
    				timings->bt.vfrontporch &&
    				(timings->bt.vbackporch ||
    				 timings->bt.vsync))) {
    		vpif_dbg(2, debug, "Timings for width, height, horizontal back porch, horizontal sync, horizontal front porch, vertical back porch, vertical sync and vertical back porch must be defined\n");
    		return -EINVAL;
    	}
    
    	vid_ch->dv_timings = *timings;
    
    	/* Configure video port timings */
    
    	std_info->eav2sav = V4L2_DV_BT_BLANKING_WIDTH(bt) - 8;
    	std_info->sav2eav = bt->width;
    
    	std_info->l1 = 1;
    	std_info->l3 = bt->vsync + bt->vbackporch + 1;
    
    	std_info->vsize = V4L2_DV_BT_FRAME_HEIGHT(bt);
    	if (bt->interlaced) {
    		if (bt->il_vbackporch || bt->il_vfrontporch || bt->il_vsync) {
    			std_info->l5 = std_info->vsize/2 -
    				(bt->vfrontporch - 1);
    			std_info->l7 = std_info->vsize/2 + 1;
    			std_info->l9 = std_info->l7 + bt->il_vsync +
    				bt->il_vbackporch + 1;
    			std_info->l11 = std_info->vsize -
    				(bt->il_vfrontporch - 1);
    		} else {
    			vpif_dbg(2, debug, "Required timing values for interlaced BT format missing\n");
    			return -EINVAL;
    		}
    	} else {
    		std_info->l5 = std_info->vsize - (bt->vfrontporch - 1);
    	}
    	strncpy(std_info->name, "Custom timings BT656/1120", VPIF_MAX_NAME);
    	std_info->width = bt->width;
    	std_info->height = bt->height;
    	std_info->frm_fmt = bt->interlaced ? 0 : 1;
    	std_info->ycmux_mode = 0;
    	std_info->capture_format = 0;
    	std_info->vbi_supported = 0;
    	std_info->hd_sd = 1;
    	std_info->stdid = 0;
    
    	vid_ch->stdid = 0;
    	return 0;
    }
    
    /**
     * vpif_g_dv_timings() - G_DV_TIMINGS handler
     * @file: file ptr
     * @priv: file handle
     * @timings: digital video timings
     */
    static int vpif_g_dv_timings(struct file *file, void *priv,
    		struct v4l2_dv_timings *timings)
    {
    	struct vpif_capture_config *config = vpif_dev->platform_data;
    	struct video_device *vdev = video_devdata(file);
    	struct channel_obj *ch = video_get_drvdata(vdev);
    	struct video_obj *vid_ch = &ch->video;
    	struct vpif_capture_chan_config *chan_cfg;
    	struct v4l2_input input;
    
    	if (!config->chan_config[ch->channel_id].inputs)
    		return -ENODATA;
    
    	chan_cfg = &config->chan_config[ch->channel_id];
    	input = chan_cfg->inputs[ch->input_idx].input;
    	if (input.capabilities != V4L2_IN_CAP_DV_TIMINGS)
    		return -ENODATA;
    
    	*timings = vid_ch->dv_timings;
    
    	return 0;
    }
    
    /*
     * vpif_log_status() - Status information
     * @file: file ptr
     * @priv: file handle
     *
     * Returns zero.
     */
    static int vpif_log_status(struct file *filep, void *priv)
    {
    	/* status for sub devices */
    	v4l2_device_call_all(&vpif_obj.v4l2_dev, 0, core, log_status);
    
    	return 0;
    }
    
    /* vpif capture ioctl operations */
    static const struct v4l2_ioctl_ops vpif_ioctl_ops = {
    	.vidioc_querycap		= vpif_querycap,
    	.vidioc_enum_fmt_vid_cap	= vpif_enum_fmt_vid_cap,
    	.vidioc_g_fmt_vid_cap		= vpif_g_fmt_vid_cap,
    	.vidioc_s_fmt_vid_cap		= vpif_s_fmt_vid_cap,
    	.vidioc_try_fmt_vid_cap		= vpif_try_fmt_vid_cap,
    
    	.vidioc_enum_input		= vpif_enum_input,
    	.vidioc_s_input			= vpif_s_input,
    	.vidioc_g_input			= vpif_g_input,
    
    	.vidioc_reqbufs			= vb2_ioctl_reqbufs,
    	.vidioc_create_bufs		= vb2_ioctl_create_bufs,
    	.vidioc_querybuf		= vb2_ioctl_querybuf,
    	.vidioc_qbuf			= vb2_ioctl_qbuf,
    	.vidioc_dqbuf			= vb2_ioctl_dqbuf,
    	.vidioc_expbuf			= vb2_ioctl_expbuf,
    	.vidioc_streamon		= vb2_ioctl_streamon,
    	.vidioc_streamoff		= vb2_ioctl_streamoff,
    
    	.vidioc_querystd		= vpif_querystd,
    	.vidioc_s_std			= vpif_s_std,
    	.vidioc_g_std			= vpif_g_std,
    
    	.vidioc_enum_dv_timings		= vpif_enum_dv_timings,
    	.vidioc_query_dv_timings	= vpif_query_dv_timings,
    	.vidioc_s_dv_timings		= vpif_s_dv_timings,
    	.vidioc_g_dv_timings		= vpif_g_dv_timings,
    
    	.vidioc_log_status		= vpif_log_status,
    };
    
    /* vpif file operations */
    static const struct v4l2_file_operations vpif_fops = {
    	.owner = THIS_MODULE,
    	.open = v4l2_fh_open,
    	.release = vb2_fop_release,
    	.unlocked_ioctl = video_ioctl2,
    	.mmap = vb2_fop_mmap,
    	.poll = vb2_fop_poll
    };
    
    /**
     * initialize_vpif() - Initialize vpif data structures
     *
     * Allocate memory for data structures and initialize them
     */
    static int initialize_vpif(void)
    {
    	int err, i, j;
    	int free_channel_objects_index;
    
    	/* Allocate memory for six channel objects */
    	for (i = 0; i < VPIF_CAPTURE_MAX_DEVICES; i++) {
    		vpif_obj.dev[i] =
    		    kzalloc(sizeof(*vpif_obj.dev[i]), GFP_KERNEL);
    		/* If memory allocation fails, return error */
    		if (!vpif_obj.dev[i]) {
    			free_channel_objects_index = i;
    			err = -ENOMEM;
    			goto vpif_init_free_channel_objects;
    		}
    	}
    	return 0;
    
    vpif_init_free_channel_objects:
    	for (j = 0; j < free_channel_objects_index; j++)
    		kfree(vpif_obj.dev[j]);
    	return err;
    }
    
    static int vpif_async_bound(struct v4l2_async_notifier *notifier,
    			    struct v4l2_subdev *subdev,
    			    struct v4l2_async_subdev *asd)
    {
    	int i;
    
    	for (i = 0; i < vpif_obj.config->asd_sizes[0]; i++) {
    		struct v4l2_async_subdev *_asd = vpif_obj.config->asd[i];
    		const struct fwnode_handle *fwnode = _asd->match.fwnode.fwnode;
    
    		if (fwnode == subdev->fwnode) {
    			vpif_obj.sd[i] = subdev;
    			vpif_obj.config->chan_config->inputs[i].subdev_name =
    				(char *)to_of_node(subdev->fwnode)->full_name;
    			vpif_dbg(2, debug,
    				 "%s: setting input %d subdev_name = %s\n",
    				 __func__, i,
    				vpif_obj.config->chan_config->inputs[i].subdev_name);
    			return 0;
    		}
    	}
    
    	for (i = 0; i < vpif_obj.config->subdev_count; i++)
    		if (!strcmp(vpif_obj.config->subdev_info[i].name,
    			    subdev->name)) {
    			vpif_obj.sd[i] = subdev;
    			return 0;
    		}
    
    	return -EINVAL;
    }
    
    static int vpif_probe_complete(void)
    {
    	struct common_obj *common;
    	struct video_device *vdev;
    	struct channel_obj *ch;
    	struct vb2_queue *q;
    	int j, err, k;
    
    	for (j = 0; j < VPIF_CAPTURE_MAX_DEVICES; j++) {
    		ch = vpif_obj.dev[j];
    		ch->channel_id = j;
    		common = &(ch->common[VPIF_VIDEO_INDEX]);
    		spin_lock_init(&common->irqlock);
    		mutex_init(&common->lock);
    
    		/* select input 0 */
    		err = vpif_set_input(vpif_obj.config, ch, 0);
    		if (err)
    			goto probe_out;
    
    		/* set initial format */
    		ch->video.stdid = V4L2_STD_525_60;
    		memset(&ch->video.dv_timings, 0, sizeof(ch->video.dv_timings));
    		common->fmt.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
    		vpif_update_std_info(ch);
    
    		/* Initialize vb2 queue */
    		q = &common->buffer_queue;
    		q->type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
    		q->io_modes = VB2_MMAP | VB2_USERPTR | VB2_DMABUF;
    		q->drv_priv = ch;
    		q->ops = &video_qops;
    		q->mem_ops = &vb2_dma_contig_memops;
    		q->buf_struct_size = sizeof(struct vpif_cap_buffer);
    		q->timestamp_flags = V4L2_BUF_FLAG_TIMESTAMP_MONOTONIC;
    		q->min_buffers_needed = 1;
    		q->lock = &common->lock;
    		q->dev = vpif_dev;
    
    		err = vb2_queue_init(q);
    		if (err) {
    			vpif_err("vpif_capture: vb2_queue_init() failed\n");
    			goto probe_out;
    		}
    
    		INIT_LIST_HEAD(&common->dma_queue);
    
    		/* Initialize the video_device structure */
    		vdev = &ch->video_dev;
    		strlcpy(vdev->name, VPIF_DRIVER_NAME, sizeof(vdev->name));
    		vdev->release = video_device_release_empty;
    		vdev->fops = &vpif_fops;
    		vdev->ioctl_ops = &vpif_ioctl_ops;
    		vdev->v4l2_dev = &vpif_obj.v4l2_dev;
    		vdev->vfl_dir = VFL_DIR_RX;
    		vdev->queue = q;
    		vdev->lock = &common->lock;
    		video_set_drvdata(&ch->video_dev, ch);
    		err = video_register_device(vdev,
    					    VFL_TYPE_GRABBER, (j ? 1 : 0));
    		if (err)
    			goto probe_out;
    	}
    
    	v4l2_info(&vpif_obj.v4l2_dev, "VPIF capture driver initialized\n");
    	return 0;
    
    probe_out:
    	for (k = 0; k < j; k++) {
    		/* Get the pointer to the channel object */
    		ch = vpif_obj.dev[k];
    		common = &ch->common[k];
    		/* Unregister video device */
    		video_unregister_device(&ch->video_dev);
    	}
    	kfree(vpif_obj.sd);
    	v4l2_device_unregister(&vpif_obj.v4l2_dev);
    
    	return err;
    }
    
    static int vpif_async_complete(struct v4l2_async_notifier *notifier)
    {
    	return vpif_probe_complete();
    }
    
    static struct vpif_capture_config *
    vpif_capture_get_pdata(struct platform_device *pdev)
    {
    	struct device_node *endpoint = NULL;
    	struct v4l2_fwnode_endpoint bus_cfg;
    	struct vpif_capture_config *pdata;
    	struct vpif_subdev_info *sdinfo;
    	struct vpif_capture_chan_config *chan;
    	unsigned int i;
    
    	/*
    	 * DT boot: OF node from parent device contains
    	 * video ports & endpoints data.
    	 */
    	if (pdev->dev.parent && pdev->dev.parent->of_node)
    		pdev->dev.of_node = pdev->dev.parent->of_node;
    	if (!IS_ENABLED(CONFIG_OF) || !pdev->dev.of_node)
    		return pdev->dev.platform_data;
    
    	pdata = devm_kzalloc(&pdev->dev, sizeof(*pdata), GFP_KERNEL);
    	if (!pdata)
    		return NULL;
    	pdata->subdev_info =
    		devm_kzalloc(&pdev->dev, sizeof(*pdata->subdev_info) *
    			     VPIF_CAPTURE_NUM_CHANNELS, GFP_KERNEL);
    
    	if (!pdata->subdev_info)
    		return NULL;
    
    	for (i = 0; i < VPIF_CAPTURE_NUM_CHANNELS; i++) {
    		struct device_node *rem;
    		unsigned int flags;
    		int err;
    
    		endpoint = of_graph_get_next_endpoint(pdev->dev.of_node,
    						      endpoint);
    		if (!endpoint)
    			break;
    
    		sdinfo = &pdata->subdev_info[i];
    		chan = &pdata->chan_config[i];
    		chan->inputs = devm_kzalloc(&pdev->dev,
    					    sizeof(*chan->inputs) *
    					    VPIF_CAPTURE_NUM_CHANNELS,
    					    GFP_KERNEL);
    		if (!chan->inputs)
    			return NULL;
    
    		chan->input_count++;
    		chan->inputs[i].input.type = V4L2_INPUT_TYPE_CAMERA;
    		chan->inputs[i].input.std = V4L2_STD_ALL;
    		chan->inputs[i].input.capabilities = V4L2_IN_CAP_STD;
    
    		err = v4l2_fwnode_endpoint_parse(of_fwnode_handle(endpoint),
    						 &bus_cfg);
    		if (err) {
    			dev_err(&pdev->dev, "Could not parse the endpoint\n");
    			goto done;
    		}
    		dev_dbg(&pdev->dev, "Endpoint %pOF, bus_width = %d\n",
    			endpoint, bus_cfg.bus.parallel.bus_width);
    		flags = bus_cfg.bus.parallel.flags;
    
    		if (flags & V4L2_MBUS_HSYNC_ACTIVE_HIGH)
    			chan->vpif_if.hd_pol = 1;
    
    		if (flags & V4L2_MBUS_VSYNC_ACTIVE_HIGH)
    			chan->vpif_if.vd_pol = 1;
    
    		rem = of_graph_get_remote_port_parent(endpoint);
    		if (!rem) {
    			dev_dbg(&pdev->dev, "Remote device at %pOF not found\n",
    				endpoint);
    			goto done;
    		}
    
    		dev_dbg(&pdev->dev, "Remote device %s, %pOF found\n",
    			rem->name, rem);
    		sdinfo->name = rem->full_name;
    
    		pdata->asd[i] = devm_kzalloc(&pdev->dev,
    					     sizeof(struct v4l2_async_subdev),
    					     GFP_KERNEL);
    		if (!pdata->asd[i]) {
    			of_node_put(rem);
    			pdata = NULL;
    			goto done;
    		}
    
    		pdata->asd[i]->match_type = V4L2_ASYNC_MATCH_FWNODE;
    		pdata->asd[i]->match.fwnode.fwnode = of_fwnode_handle(rem);
    		of_node_put(rem);
    	}
    
    done:
    	if (pdata) {
    		pdata->asd_sizes[0] = i;
    		pdata->subdev_count = i;
    		pdata->card_name = "DA850/OMAP-L138 Video Capture";
    	}
    
    	return pdata;
    }
    
    /**
     * vpif_probe : This function probes the vpif capture driver
     * @pdev: platform device pointer
     *
     * This creates device entries by register itself to the V4L2 driver and
     * initializes fields of each channel objects
     */
    static __init int vpif_probe(struct platform_device *pdev)
    {
    	struct vpif_subdev_info *subdevdata;
    	struct i2c_adapter *i2c_adap;
    	struct resource *res;
    	int subdev_count;
    	int res_idx = 0;
    	int i, err;
    
    	pdev->dev.platform_data = vpif_capture_get_pdata(pdev);
    	if (!pdev->dev.platform_data) {
    		dev_warn(&pdev->dev, "Missing platform data.  Giving up.\n");
    		return -EINVAL;
    	}
    
    	if (!pdev->dev.platform_data) {
    		dev_warn(&pdev->dev, "Missing platform data.  Giving up.\n");
    		return -EINVAL;
    	}
    
    	vpif_dev = &pdev->dev;
    
    	err = initialize_vpif();
    	if (err) {
    		v4l2_err(vpif_dev->driver, "Error initializing vpif\n");
    		return err;
    	}
    
    	err = v4l2_device_register(vpif_dev, &vpif_obj.v4l2_dev);
    	if (err) {
    		v4l2_err(vpif_dev->driver, "Error registering v4l2 device\n");
    		return err;
    	}
    
    	while ((res = platform_get_resource(pdev, IORESOURCE_IRQ, res_idx))) {
    		err = devm_request_irq(&pdev->dev, res->start, vpif_channel_isr,
    					IRQF_SHARED, VPIF_DRIVER_NAME,
    					(void *)(&vpif_obj.dev[res_idx]->
    					channel_id));
    		if (err) {
    			err = -EINVAL;
    			goto vpif_unregister;
    		}
    		res_idx++;
    	}
    
    	vpif_obj.config = pdev->dev.platform_data;
    
    	subdev_count = vpif_obj.config->subdev_count;
    	vpif_obj.sd = kcalloc(subdev_count, sizeof(*vpif_obj.sd), GFP_KERNEL);
    	if (!vpif_obj.sd) {
    		err = -ENOMEM;
    		goto vpif_unregister;
    	}
    
    	if (!vpif_obj.config->asd_sizes[0]) {
    		int i2c_id = vpif_obj.config->i2c_adapter_id;
    
    		i2c_adap = i2c_get_adapter(i2c_id);
    		WARN_ON(!i2c_adap);
    		for (i = 0; i < subdev_count; i++) {
    			subdevdata = &vpif_obj.config->subdev_info[i];
    			vpif_obj.sd[i] =
    				v4l2_i2c_new_subdev_board(&vpif_obj.v4l2_dev,
    							  i2c_adap,
    							  &subdevdata->
    							  board_info,
    							  NULL);
    
    			if (!vpif_obj.sd[i]) {
    				vpif_err("Error registering v4l2 subdevice\n");
    				err = -ENODEV;
    				goto probe_subdev_out;
    			}
    			v4l2_info(&vpif_obj.v4l2_dev,
    				  "registered sub device %s\n",
    				   subdevdata->name);
    		}
    		vpif_probe_complete();
    	} else {
    		vpif_obj.notifier.subdevs = vpif_obj.config->asd;
    		vpif_obj.notifier.num_subdevs = vpif_obj.config->asd_sizes[0];
    		vpif_obj.notifier.bound = vpif_async_bound;
    		vpif_obj.notifier.complete = vpif_async_complete;
    		err = v4l2_async_notifier_register(&vpif_obj.v4l2_dev,
    						   &vpif_obj.notifier);
    		if (err) {
    			vpif_err("Error registering async notifier\n");
    			err = -EINVAL;
    			goto probe_subdev_out;
    		}
    	}
    
    	return 0;
    
    probe_subdev_out:
    	/* free sub devices memory */
    	kfree(vpif_obj.sd);
    vpif_unregister:
    	v4l2_device_unregister(&vpif_obj.v4l2_dev);
    
    	return err;
    }
    
    /**
     * vpif_remove() - driver remove handler
     * @device: ptr to platform device structure
     *
     * The vidoe device is unregistered
     */
    static int vpif_remove(struct platform_device *device)
    {
    	struct channel_obj *ch;
    	int i;
    
    	v4l2_device_unregister(&vpif_obj.v4l2_dev);
    
    	kfree(vpif_obj.sd);
    	/* un-register device */
    	for (i = 0; i < VPIF_CAPTURE_MAX_DEVICES; i++) {
    		/* Get the pointer to the channel object */
    		ch = vpif_obj.dev[i];
    		/* Unregister video device */
    		video_unregister_device(&ch->video_dev);
    		kfree(vpif_obj.dev[i]);
    	}
    	return 0;
    }
    
    #ifdef CONFIG_PM_SLEEP
    /**
     * vpif_suspend: vpif device suspend
     */
    static int vpif_suspend(struct device *dev)
    {
    
    	struct common_obj *common;
    	struct channel_obj *ch;
    	int i;
    
    	for (i = 0; i < VPIF_CAPTURE_MAX_DEVICES; i++) {
    		/* Get the pointer to the channel object */
    		ch = vpif_obj.dev[i];
    		common = &ch->common[VPIF_VIDEO_INDEX];
    
    		if (!vb2_start_streaming_called(&common->buffer_queue))
    			continue;
    
    		mutex_lock(&common->lock);
    		/* Disable channel */
    		if (ch->channel_id == VPIF_CHANNEL0_VIDEO) {
    			enable_channel0(0);
    			channel0_intr_enable(0);
    		}
    		if (ch->channel_id == VPIF_CHANNEL1_VIDEO ||
    			ycmux_mode == 2) {
    			enable_channel1(0);
    			channel1_intr_enable(0);
    		}
    		mutex_unlock(&common->lock);
    	}
    
    	return 0;
    }
    
    /*
     * vpif_resume: vpif device suspend
     */
    static int vpif_resume(struct device *dev)
    {
    	struct common_obj *common;
    	struct channel_obj *ch;
    	int i;
    
    	for (i = 0; i < VPIF_CAPTURE_MAX_DEVICES; i++) {
    		/* Get the pointer to the channel object */
    		ch = vpif_obj.dev[i];
    		common = &ch->common[VPIF_VIDEO_INDEX];
    
    		if (!vb2_start_streaming_called(&common->buffer_queue))
    			continue;
    
    		mutex_lock(&common->lock);
    		/* Enable channel */
    		if (ch->channel_id == VPIF_CHANNEL0_VIDEO) {
    			enable_channel0(1);
    			channel0_intr_enable(1);
    		}
    		if (ch->channel_id == VPIF_CHANNEL1_VIDEO ||
    			ycmux_mode == 2) {
    			enable_channel1(1);
    			channel1_intr_enable(1);
    		}
    		mutex_unlock(&common->lock);
    	}
    
    	return 0;
    }
    #endif
    
    static SIMPLE_DEV_PM_OPS(vpif_pm_ops, vpif_suspend, vpif_resume);
    
    static __refdata struct platform_driver vpif_driver = {
    	.driver	= {
    		.name	= VPIF_DRIVER_NAME,
    		.pm	= &vpif_pm_ops,
    	},
    	.probe = vpif_probe,
    	.remove = vpif_remove,
    };
    
    module_platform_driver(vpif_driver);
    

  • manisha, thank you for your reply.

    I will check the attached file.

    Thank you very much.