This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6424 Problems with Cache Chip Support Include Files



I'm working on a C6424 DSP and need to incorporate the "csl_cache.h" include file to take care of caching issues.  Unfortunately, when you do that, "csl_cache.h" references "csl_chiphal.h" which causes the compilation to fail.  "csl_chiphal.h" does not have support for the C6424 chip.

Is there a standard work around to this problem?

What led to this discovery is that if you integrate the NDK with an app that uses DMA transfer to/from the UARTs, the CPU doesn't see the data transfered by the EDMA3 controller.  The transfer buffer in cache is apparently not updated.

Mike