This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Davinci 6467T EVM setup

I have a 6467T EVM with a TV attached to the YPbPr output and a DVD player attached to the YPbPr input.  On startup, I get the demo screen on the TV and I can play the compressed video files included with the demo with the remote control.  I cannot record the input from the DVD player (or see it on the screen).  One thing that I noticed was that the shipping configuration for the EVM dip switches had 1,2, and 3 on and the rest off.  This is different from the docs that came with the board which had 2,3, and 4 set to on.  However, the shipping configuration boots to the demo screen and the doc settings do not.