Part Number: AM6548
Other Parts Discussed in Thread: TMDSLCD1EVM
Tool/software: Linux
Hi Experts,
I've run Matrix GUI on TMDX654GPEVM and TMDSLCD1EVM.
When I press the Dhrystone icon, the following result is displayed at the bottom of the LCD.
CPU clock = 400 MHz
Dhrystone DMIPS/MHz = 5.9
Is this result correct? I think Cortex-A53 should be 2.3 DMIPS/MHz. Additionally, CPU clock is 400 MHz.
According to the top command, it seems that the Dhrystone calculation is processed on cpu2 or cpu3.
Also, the same result is obtained with the included SD card and the rebuilt SD card by PSDK-Linux v5.1.
Please give me some advice.
Regards,
Kzk