Other Parts Discussed in Thread: OMAP-L137
Hi:
Evaluation Board: Digital Spectrum, OMAP-L137 EVM Rev1.
Software: MS Viusal studio 2005 with Windows CE6.0 R3 platform builder. And WINCE BSP for OMPA-L137 get from MPC Data.
Test cases for "Serial Flasher Host Program" for OMP-L137 with OMAP-L137 Rev1.
(1) sfh_OMAP-L137-1-50 -spiflash_dsp -p Com5 -appStartAddr 0xC3F60000 -appLoadAddr 0xC3F60000 dsp-spi-ais.bin ubl-spi.bin EBOOTSPIFLASH.nb0(Rev1)
Worked fine, system boot up OK. Serial Flasher Host Program v1.50 work fine with OMAP-L137 Rev1.
(2) sfh_OMAP-L137-1-67 -flash_dsp -p Com5 -baud 230400 -targetType OMAPL137_v1 -appStartAddr 0xC3F60000 -appLoadAddr 0xC3F60000 dsp-spi-ais.bin ubl-spi.bin EBOOTSPIFLASH.nb0(Rev1)
Downloaded OK, however could not boot.
We are developing a system board with OMAP-L137 Rev2.
We have changed SOC Type to OMAP-L137 Rev2 in the platform builder to create new EBOOTSPIFLASH.NB0 for OMAP-L137 Rev2.
ubl_C6747_SPI_MEM.bin ubl_OMAPL137_v2_SPI_MEM.bin came with "OMAP-L137_FlashAndBootUtils_2_15".
I tried to flash the system to OMAP-L137 Rev2:
(3) sfh_OMAP-L137-1-67 -flash_dsp -p Com5 -appStartAddr 0xC3F60000 -appLoadAddr 0xC3F60000 dsp-spi-ais.bin ubl-spi.bin EBOOTSPIFLASH.nb0(Rev2)
Downloaded OK, however could not boot.
(4) sfh_OMAP-L137-1-67 -flash_dsp -p Com5 -appStartAddr 0xC3F60000 -appLoadAddr 0xC3F60000 ubl_C6747_SPI_MEM.bin ubl_OMAPL137_v2_SPI_MEM.bin EBOOTSPIFLASH.nb0(Rev2)
Downloaded OK, however could not boot.
Questions:
A. Why Case# (2) doesn't work?
B. Do dsp-spi-ais.bin and ubl-spi.bin work on OMAP-L137 Rev2 as well as Rev1?
C. Did I use the programs correctly on case#(3), case#(4)?
D. Did I miss something important?
Thank you for your help.
-kc