This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSL for DM6446



Where can I find the CSL lib for DM6446?

The current CSL version I have does not include DM6446.  It only supports up to DM642x.

Thanks

  • There is no CSL for the DM6446 (one was never written), what was the CSL in prior devices has effectively been replaced by the peripheral support package (PSP) which is made up of vaious Linux device drivers which is included in the DVSDK. This is one of the reasons that only high level OSes such as Linux are supported on the ARM through TI, though some third parties offer device support packages for other OSes such as Windows CE.

  • Unfortunately, there is no CSL available for DM6446; this is primarily because all the drivers (and corresponding header files with register definitions) are ARM/LINUX based.