Hi TI Experts,
Please let me confirm the following question.
[Question]
Can customer reduce the capacitors on the unused AM574x functions(like DPS, IVA, GPU and so on) power line?
For example, if customer will not use the following feature on AM5746 device.
GPU、IVA、DSP, DDR2、HDMI、SATA
Can they reduce the capacitors on below lines?
・VDD_GPU 10uF×2、0.01uF×6
・VDD_IVA 10uF×2、0.01uF×4
・VDD_DSPEVE 47uF×1、10uF×2、0.01uF×8
・VDDS_DDR2 100uF×1、10uF×1、0.01uF×8
・VDDA_HDMI 1uF×1、0.1uF×1、0.01uF×1
・VDDA_SATA 1uF×1、0.1uF×1、0.01uF×1
If you have any questions, please let me know.
Best regards.
Kaka